KEA64 Watchdog Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA64 Watchdog Clock

1,223件の閲覧回数
leekate-b45752
NXP Employee
NXP Employee

Hello, 

When using 1kHz(Internal low power oscillator) for watchdog clock, the tolerance is about -33% to 25% according to the spec as below, so the error for the reset time of watchdog timeout is too big. Is there way to reduce it? Should I change the watchdog clock in order to reduce the to tolerance? 

leekate-b45752_0-1612244522151.png

 

Best regards,

Kate Lee

ラベル(1)
0 件の賞賛
返信
0 返答(返信)