KEA64 Watchdog Clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA64 Watchdog Clock

1,188 Views
leekate-b45752
NXP Employee
NXP Employee

Hello, 

When using 1kHz(Internal low power oscillator) for watchdog clock, the tolerance is about -33% to 25% according to the spec as below, so the error for the reset time of watchdog timeout is too big. Is there way to reduce it? Should I change the watchdog clock in order to reduce the to tolerance? 

leekate-b45752_0-1612244522151.png

 

Best regards,

Kate Lee

Labels (1)
0 Kudos
Reply
0 Replies