KEA32 Downloading binary to target...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA32 Downloading binary to target...

1,904件の閲覧回数
cheolminlee
Contributor II

Hi,

I used Codewarrior 10.7.

I use KEA32 but the program can not be downloaded.

Downloading binary to target...

I know that the header file is wrong and I have tried it with other KEA series header files.

Help me...

0 件の賞賛
返信
3 返答(返信)

1,824件の閲覧回数
cheolminlee
Contributor II

Hi,

Thank you for your reply.

I am using KEA32 as a 32pin. Making PCB

When I download the program, I get up to 100%, but 'downloading binary to target ...'

I don't know that...

0 件の賞賛
返信

1,824件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi CheolMin Lee

Could you describe more what is the error that you get when you try to download the binary. What do you mean with I have tried it with other KEA series header files.?

You shouldn't change the header file that code warrior generate when you create the project, so please describe more your issue.

Best Regards

Jorge Alcala

0 件の賞賛
返信

1,824件の閲覧回数
mjbcswitzerland
Specialist V

Hi

I believe that S32 Design Studio is what tends to be used with the KEA32 - I don't know that CW10.7 supports programming and debugging it(?)
Try a binary from here in case you think it may be a problem with the binary being used: http://www.utasker.com/kinetis/FRDM-KEAZN32Q64.html

Regards

Mark

0 件の賞賛
返信