KEA128 Peripheral description .svd File

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KEA128 Peripheral description .svd File

跳至解决方案
2,144 次查看
ProfDrTwix
Contributor I

I have to debug multiple projects with a KEA128. To read the peripheral description in VSCode with the extension Cortex-Debug I need a .svd file. Is there already a exisiting .svd - file? I searched within the SDK and wasn´t able to find one neither is one available online.

Thanks in advance.

0 项奖励
回复
1 解答
2,128 次查看
ErichStyger
Specialist I

I don't do any development for the KEA128, but there are SVD files available for KDS you should be able to use. The are available on SourceForge, see https://mcuoneclipse.com/2014/09/27/updated-eclipse-embsysreg-viewer-with-extra-freescale-svd-files/

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,129 次查看
ErichStyger
Specialist I

I don't do any development for the KEA128, but there are SVD files available for KDS you should be able to use. The are available on SourceForge, see https://mcuoneclipse.com/2014/09/27/updated-eclipse-embsysreg-viewer-with-extra-freescale-svd-files/

I hope this helps,

Erich

0 项奖励
回复
2,130 次查看
JRoberto
NXP TechSupport
NXP TechSupport

Hello @ProfDrTwix ,

I searched for the KEA's SVD file and unfortunately it seems like it doesn't exist.

0 项奖励
回复