KEA128 Peripheral description .svd File

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA128 Peripheral description .svd File

ソリューションへジャンプ
2,149件の閲覧回数
ProfDrTwix
Contributor I

I have to debug multiple projects with a KEA128. To read the peripheral description in VSCode with the extension Cortex-Debug I need a .svd file. Is there already a exisiting .svd - file? I searched within the SDK and wasn´t able to find one neither is one available online.

Thanks in advance.

0 件の賞賛
返信
1 解決策
2,133件の閲覧回数
ErichStyger
Specialist I

I don't do any development for the KEA128, but there are SVD files available for KDS you should be able to use. The are available on SourceForge, see https://mcuoneclipse.com/2014/09/27/updated-eclipse-embsysreg-viewer-with-extra-freescale-svd-files/

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,134件の閲覧回数
ErichStyger
Specialist I

I don't do any development for the KEA128, but there are SVD files available for KDS you should be able to use. The are available on SourceForge, see https://mcuoneclipse.com/2014/09/27/updated-eclipse-embsysreg-viewer-with-extra-freescale-svd-files/

I hope this helps,

Erich

0 件の賞賛
返信
2,135件の閲覧回数
JRoberto
NXP TechSupport
NXP TechSupport

Hello @ProfDrTwix ,

I searched for the KEA's SVD file and unfortunately it seems like it doesn't exist.

0 件の賞賛
返信