KEA128 Peripheral description .svd File

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA128 Peripheral description .svd File

Jump to solution
2,207 Views
ProfDrTwix
Contributor I

I have to debug multiple projects with a KEA128. To read the peripheral description in VSCode with the extension Cortex-Debug I need a .svd file. Is there already a exisiting .svd - file? I searched within the SDK and wasn´t able to find one neither is one available online.

Thanks in advance.

0 Kudos
Reply
1 Solution
2,191 Views
ErichStyger
Specialist I

I don't do any development for the KEA128, but there are SVD files available for KDS you should be able to use. The are available on SourceForge, see https://mcuoneclipse.com/2014/09/27/updated-eclipse-embsysreg-viewer-with-extra-freescale-svd-files/

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
2 Replies
2,192 Views
ErichStyger
Specialist I

I don't do any development for the KEA128, but there are SVD files available for KDS you should be able to use. The are available on SourceForge, see https://mcuoneclipse.com/2014/09/27/updated-eclipse-embsysreg-viewer-with-extra-freescale-svd-files/

I hope this helps,

Erich

0 Kudos
Reply
2,193 Views
JRoberto
NXP TechSupport
NXP TechSupport

Hello @ProfDrTwix ,

I searched for the KEA's SVD file and unfortunately it seems like it doesn't exist.

0 Kudos
Reply