KEA128 PWT help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,811件の閲覧回数
maharajshreekum
Contributor III

Hi all,

I am trying to measure the pulse width of PWM using PWT (Pulse Width Timer) module of KEA128. The frequency which I am measuring is 1Khz(50% duty cycle, can be changed) on PTD5 (PWINT0 channel). I have configured the PWT with bus clock of 20Mhz and pre-scale of 64. I have also enabled the interrupts for Data Ready and PWT interrupt so as to read the PPW (Positive Pulse width) and NPW (Negative PW) values in Reg PWT_R1 and PWT_R2,summing both value to count of one period.

Below is the  my code

/************************************************************************************************************/

void PWT_Init(void)
{
SIM_SCGC |= SIM_SCGC_PWT_MASK; /* Enable Clock for PWT module */

PWT_R1 |= PWT_R1_PWTEN_MASK; /* Enable PWT module*/
PWT_R1 |= PWT_R1_PRE(6); /* Set Prescaler: 64. 20 Mhz/64= 312.5KHz.*/

PWT_R1 |= PWT_R1_EDGE(2); /* first falling edge starts measurement, and on all the subsequent rising and falling edges*/
PWT_R1 |= PWT_R1_PWTSR_MASK; /* Soft module reset */
PWT_R1 |= PWT_R1_PRDYIE_MASK; /* PWT Pulse Width Data Ready Int Enable*/
PWT_R1 |= PWT_R1_PWTIE_MASK; /* PWT Module Interrupt Enable*/

SIM_PINSEL1 &= ~SIM_PINSEL1_PWTIN0PS_MASK; /* PWT channel mapped to pin PTD5 (PWINT0) */
}

ISR of PWT is, I have enabled NVIC and all in main......

void PWT_IRQHandler()
{
if (((PWT_R1 & PWT_R1_PWTRDY_MASK)>>PWT_R1_PWTRDY_SHIFT == 1))
{
LED0_TOGGLE;
pwm_rd = (PWT_R2 & PWT_R2_NPW_MASK) >> PWT_R2_NPW_SHIFT;
pwm_rd1 = (PWT_R1 & PWT_R1_PPW_MASK);
}
PWT_R1 &= ~PWT_R1_PWTRDY_MASK; /* Clear flag: read reg then write 0 to PWTRDY */
}

/************************************************************************************************************/

Now, My problem is that when i am trying to print values of both NPW and PPW in main, only NPW is getting updated but not PPW. PPW is also NOT getting updated even when I change EDGE[1:0] bits to PWT_R1_EDGE(1);

For 1Khz input pulse width, the value in NPW is 156, it should be 156 in PPW so that I can calculate how much is the  duty cycle of the PWM pulse.

Freq. can be calculated as below 

PWT Clock / (PPW ? NPW), PWT Clock = 20Mhz/64 = 312500/312 = 1000 (!Khz pwm)

Pls shed some light on this, if anybody has done this before. WHERE I AM GOING WRONG!!!!

0 件の賞賛
返信
1 解決策
2,485件の閲覧回数
maharajshreekum
Contributor III

Hi Robin,

thanks for the reply.

@The pwm_rd and pwm_rd1 in your PWT_IRQHandler() seems to be error.

here pwm_rd and pwm_rd1 are two diffrent uint16_t volatile variables (used in ISR) which i use to get values from NPW and PPW registers.

@o not change any PWT configurations as long as PWTEN is set.

Now I have changed that line and enabled tha PWT module after configuring the PWT(clock,egde etc..)

But still, I am not bale to get the result. The thing is that PPW val is not getting update in any case whenever I change the selection bits of EDGE[1:0]. 

ISR is gettting serviced,vals are being printed but only of NPW....

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,485件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The pwm_rd and pwm_rd1 in your PWT_IRQHandler() seems to be error. Should be like below:

        u32PositivePulse = (PWT_R1 & PWT_R1_PPW_MASK)>> PWT_R1_PPW_SHIFT;
        u32NegativePulse = (PWT_R2 & PWT_R2_NPW_MASK) ;

To avoid unexpected behavior, do not change any PWT configurations as long as PWTEN is set. I saw that you enabled that bit at the beginning of PWT_Init().

I think you can refer the PWT_Init() in pwt.c.

pwtc.png

The pwt.c can be found in below folder. For example: ...:\Program Files\Freescale\S32DS_ARM_v1.3\S32DS\S32_SDK_KEA_1_0_0\sources

pwt in S32_SDK_KEA_1_0_0.png

The S32 Design Studio for ARM v1.3 IDE can be download from here.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,486件の閲覧回数
maharajshreekum
Contributor III

Hi Robin,

thanks for the reply.

@The pwm_rd and pwm_rd1 in your PWT_IRQHandler() seems to be error.

here pwm_rd and pwm_rd1 are two diffrent uint16_t volatile variables (used in ISR) which i use to get values from NPW and PPW registers.

@o not change any PWT configurations as long as PWTEN is set.

Now I have changed that line and enabled tha PWT module after configuring the PWT(clock,egde etc..)

But still, I am not bale to get the result. The thing is that PPW val is not getting update in any case whenever I change the selection bits of EDGE[1:0]. 

ISR is gettting serviced,vals are being printed but only of NPW....

0 件の賞賛
返信
2,485件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please see the Register of PWT_R1 and PWT_R2 first.

The PositivePulse = (PWT_R1 & PWT_R1_PPW_MASK)>> PWT_R1_PPW_SHIFT; due to it's located at the higher 16bits.

PPW PWT_R1.png

The NegativePulse = (PWT_R2 & PWT_R2_NPW_MASK) ; due to it's located at the lower 16bits.

NPW PWT_R2.png

Best Regards,

Robin

2,485件の閲覧回数
maharajshreekum
Contributor III

OHHH!!!...Thanks Robin...I just misread the registers,a very basic mistake....

Thanks a lot....

0 件の賞賛
返信