KEA128 MSCAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA128 MSCAN

1,747 Views
sharadmehta
Contributor I

Need Keil example code/project to read and write CAN Messages.

Board TRK-KEA128

Labels (1)
0 Kudos
Reply
1 Reply

1,528 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello,

Hi Sharad Mehta,

   This is the same question as your another post:

KEA128 MSCAN 

  Please check that post, I have answered you.

  You can use the CW project, or you create the KEIL KEA project, then add the CW CAN driver to your keil project, it also works.

  After you create the keil project, and add the MSCAN driver have problems, please let me know.


Have a great day,
kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply