KEA128 GPIO at 1.4V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA128 GPIO at 1.4V

1,854 Views
vigneshbalaji
Senior Contributor I

Hi,

    I want to know under what conditions does KEA128 GPIO pins stay at 1.4 volts?

0 Kudos
Reply
3 Replies

1,735 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

   You already ask the same two questions in the case, I post the reply in the case directly.

  Please try to add an external pull up in the according pin which you are using, then check the voltage again.
On board output high, then other board configure the pin as GPIO input, take care, don't configure both board 1 and board 2 pin in GPIO output toghether.
You must configure on is GPIO output, another on is GPIO input.
take an example, board 1 output higher, board 2 is the GPIO input.
Add an external 10K pull up resistor between the board 1 and board 2, then test the voltage again, whether you still get 1.5V or you can get 3.3V.
Please test it at first.
Any updated information, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,735 Views
vigneshbalaji
Senior Contributor I

Hi Kerry,

               Can you tell me the reason why i should add a 10K pull up inbetween output of board 1 and input of board 2. I want to configure software wise whether to pull up input of board 1 or pull down input of board 1.

0 Kudos
Reply

1,735 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

  Do you try my suggestions?
And I don't know, whether you enable the internal pull up.
If you already enable the internal pull up, I think the problem is caused by the weak internal pull up resistor.
If you don't enable the internal pull up before, you also can try to enable the internal pull up resistor in PORT_PUEn register.
Please try it on your side, whether it works or not?
If it works, your problem is caused by the weak pull up or no pull up, the pin can't be pull to VDD because no pull up resistor.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply