KEA 64 FOC SINGLE SHUNT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA 64 FOC SINGLE SHUNT

2,079件の閲覧回数
LiXiaoQuan
Contributor I

I want to develop a single resistance FOC on the KEA64 . Is it possible?

0 件の賞賛
返信
1 返信

2,025件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

It is possible to use single shunt resistor and connect the shunt resistor  to reconstruct 3 phase current, but it is complex, especially when the state current is small or two PWM signal edge happens synchronously.

I attach DRM153.pdf, although the AN uses eFlexWM to generate PWM, but it also adapts to FTM which the K64 uses to generate PWM.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信