KEA 64 FOC SINGLE SHUNT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KEA 64 FOC SINGLE SHUNT

2,076 次查看
LiXiaoQuan
Contributor I

I want to develop a single resistance FOC on the KEA64 . Is it possible?

0 项奖励
回复
1 回复

2,022 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

It is possible to use single shunt resistor and connect the shunt resistor  to reconstruct 3 phase current, but it is complex, especially when the state current is small or two PWM signal edge happens synchronously.

I attach DRM153.pdf, although the AN uses eFlexWM to generate PWM, but it also adapts to FTM which the K64 uses to generate PWM.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复