KE18F ECC 1-Bit Correction and 3-Bit Detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE18F ECC 1-Bit Correction and 3-Bit Detection

983 Views
sean_dvorscak
Contributor III
I am looking for some documentation about whether or not the KE18F automatically fixes all 1-Bit ECC errors. The manual does not say anything about correcting the 1-Bit errors, but AN5332 says, "detection and correction of up to a 1-bit error". If the KE18F is fixing these 1-bit errors, is there a way to stop it from correcting and only report them? There is a bit of concern about 3-Bit errors looking like 1-Bit errors, and would like for it not to try and fix anything in that instance. Just report it.
0 Kudos
Reply
1 Reply

976 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi sean,

ECC function can't be modify or close in KE18F. ECC function is not like CRC. There bit error are sure can be found.

 

Regards,

Jing

0 Kudos
Reply