KE16F Vs. KE18F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KE16F Vs. KE18F

2,722件の閲覧回数
JRIIS
NXP Employee
NXP Employee

Customer asking about the implication from a technical point of view if they change their design from the MKE16F to the MKE18F.

This should be the same die so it should be fine to use both as long at they compile to the actual version.

Could I kindly ask for validation on this please?

Thanks,

/Jakob

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,702件の閲覧回数
JRIIS
NXP Employee
NXP Employee

Hi Jing,

I need to understand all deference in detailed, when you say main difference is memory size then you indicate that there is other deference. Could you please point those out?

Thanks,

/Jakob

0 件の賞賛
返信

2,693件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

KE18F has 2 CAN while KE16F has 1 CAN.

That's all I think.

 

Regards,

Jing

0 件の賞賛
返信

2,711件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Jakob,

Yes. Their main difference is memory size.

 

Regards,

Jing

0 件の賞賛
返信