KE06 Z128 Uart Bootloader (someone have bootloader?)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE06 Z128 Uart Bootloader (someone have bootloader?)

4,033 Views
donghoha
Contributor II

Hi.

I am studying Kinetis KE06.

I use custom KE06 test board(not FRDM-KE06).

Now, I need UART bootloader for KE06.

Anyone have Uart bootloader for KE06?

I desperately need this.

Thank you.

-----------------------------------------------------------------------------------

I succeed KE06 uart bootloader by AN4767SW and AN5219SW.

AN4767SW is KE02 uart bootloader program.

AN5219SW is KE06 can bootloader program.

I use IAR Embedded wrokbech.

I used AN5219SW base.

And I bring source code from AN4767SW.

It works well.

But MCU information is wrong.

Next, application program need proper icf file.

It can get from AN5219SW application config file  KE0X_128K_bootloader.icf

Labels (1)
5 Replies

3,392 Views
pokermagalli
Contributor I

Hi donghoha‌,

I'm trying to develop the same application for the same micro, but I'm using MCUXpresso IDE.

Do you think that a file similar to  KE0X_128K_bootloader.icf is needed to make it work or there are other ways to set the MCU information?

Thank you.

0 Kudos
Reply

3,392 Views
mjbcswitzerland
Specialist V

Hi Simone

See the appendix of http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf for a list of things to consider to achieve boot loader compatibility.

You can get an immediate solution for MCUXpresso on GitHub or if you are developing professionally a supported solution at http://www.utasker.com/kinetis/FRDM-KE06Z.html

Regards

Mark

0 Kudos
Reply

3,392 Views
pokermagalli
Contributor I

Thank you for the answer, it's not for professionally developing, I just to implement the bootloader feature through AN2295 in my KE06 projects. 

Are there really example code on GitHub? In which repository?  

Thank you very much

0 Kudos
Reply

3,392 Views
mjbcswitzerland
Specialist V

Hi Simone

Yes, you can get AN2295 boot loaders for almost all Kinetis parts at https://github.com/uTasker/uTasker-Kinetis (as well as KBOOT 2.0 loaders, iHex and SREC too) so no one needs to repeat porting exercises unless they are specifically doing it to learn certain things in the process. The project however also makes learning easier and more efficient because it allows you to simulate the KE06 (or other derivatives) in Visual Studio in real-time, so debugging and analysis is much quicker.

The professional version adds additional features like AES256 encryption and personal project support but is only needed when developments need to be guaranteed and kept as efficient and cost effective as possible.

Regards

Mark

0 Kudos
Reply

3,392 Views
mjbcswitzerland
Specialist V


Hi

Kboot, SREC, IHEX, AN2295 Developer's loader, Modbus slave UART loaders for KE06 (as well as I2C slave, SD card) are included in the uTasker project:
http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf
http://www.utasker.com/kinetis.html
http://www.utasker.com/kinetis/FRDM-KE06Z.html

Regards

Mark


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html