KE06 NMI pull-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE06 NMI pull-up

Jump to solution
2,061 Views
davidsherman
Senior Contributor I

I'm trying to solve a little mystery.  The pin PTB4 is also the /NMI pin.  On reset, the internal pull-up is disabled in the PORT_PUE0 register.  On the FRDM-KE06 board, there does not appear to be a pull up resistor in the schematic, and I can't find one on the board.  There appears to be some pull-up somewhere, because I can measure 3 volts on the pin on the Freedom board.  So, is there some pull up that's on by default, or is there a resistor on the schematic that I'm not seeing?  In short, can the pin be left disconnected as it appears to be on the Freedom board, or does it need to have a pull-up resistor supplied?

0 Kudos
Reply
1 Solution
1,784 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, David

In KE06 reference manual, you can find

NMI Pin Enable

This write-once field can be written after any reset. When NMIE is set, the PTB4/KBI0_P12/FTM2_CH4/SPI0_MISO/ACMP1_IN2/NMI pin functions as NMI.This pin defaults to NMI following an MCU POR. Other resets will not affect this bit. When NMIE is set, an internal pullup device on NMI is enabled. And this bit default value is 1. So this pin has internal pull-up resistor.

Hope my reply can help you.

Best Regards

Paul

View solution in original post

0 Kudos
Reply
2 Replies
1,784 Views
davidsherman
Senior Contributor I

Ah, thank you!  I had missed it in that part.

0 Kudos
Reply
1,785 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, David

In KE06 reference manual, you can find

NMI Pin Enable

This write-once field can be written after any reset. When NMIE is set, the PTB4/KBI0_P12/FTM2_CH4/SPI0_MISO/ACMP1_IN2/NMI pin functions as NMI.This pin defaults to NMI following an MCU POR. Other resets will not affect this bit. When NMIE is set, an internal pullup device on NMI is enabled. And this bit default value is 1. So this pin has internal pull-up resistor.

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply