KE04 RESET pin handling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE04 RESET pin handling

Jump to solution
1,374 Views
jun1
Contributor V

I am always indebted.
As for the title, the KE04(MKE04Z128VLD4) reset pin, is it okay if it is left open if only power-on reset is used?
If opening is not desirable, do you need to connect something like CR to the terminals? Please tell us the recommended constants in that case.


Thank you.

0 Kudos
Reply
1 Solution
1,325 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi jun yamada 

  To boot normally, please add 4.7K to 10K external pull up in the reset pin, and 0.1uf capacitor to ground.

  Normally, use the above setting, will has no issue, but if you just leave it open, your boot may be failed.

   To work stably, please add the external component.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,326 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi jun yamada 

  To boot normally, please add 4.7K to 10K external pull up in the reset pin, and 0.1uf capacitor to ground.

  Normally, use the above setting, will has no issue, but if you just leave it open, your boot may be failed.

   To work stably, please add the external component.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,325 Views
jun1
Contributor V

Thank you very much.
OK.

Have a nice day.

jun

0 Kudos
Reply