KE02Z64xxx4 10M osc startup problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KE02Z64xxx4 10M osc startup problem

1,867件の閲覧回数
rqbh
Contributor III

Hi, i have a customer board using ke02z64xxx4 with a 10M osc, but it cann't startup in FEE mode until you touch it using hand,

Does anyone met the same problem ? how can i find out what reason cause this problem?

thanks.

QQ图片20150619091344.png

QQ图片20150619091517.png

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,725件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Kevin,

In this case I would like to recommend the following documentation in order to improve your application:

1. Crystal Oscillator Troubleshooting Guide

2. Microcontroller Oscillator Circuit Design Considerations

Hope this material will be useful for you.

Have an excellent day :smileyhappy:

David Diaz

0 件の賞賛
返信

1,725件の閲覧回数
danielecortella
Contributor V

Hi,

try to put a 1Mohm resistor in parallel to the oscillator (between Extal and Xtal)

0 件の賞賛
返信

1,725件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Make sure the high-/low gain mode is correctly set in OSC_CR

OSC_CR_HGO should be used with high loading and a feedback resistor but should not be set when there is no feedback resistor.

Regrds

Mark

Kinetis: µTasker Kinetis support

KE: µTasker FRDM-KE02Z support  / µTasker FRDM-KE02Z40M support  / µTasker FRDM-KE06Z support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信