KE02Z64xxx4 10M osc startup problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE02Z64xxx4 10M osc startup problem

1,868 Views
rqbh
Contributor III

Hi, i have a customer board using ke02z64xxx4 with a 10M osc, but it cann't startup in FEE mode until you touch it using hand,

Does anyone met the same problem ? how can i find out what reason cause this problem?

thanks.

QQ图片20150619091344.png

QQ图片20150619091517.png

Labels (1)
0 Kudos
Reply
3 Replies

1,726 Views
david_diaz
NXP Employee
NXP Employee

Hello Kevin,

In this case I would like to recommend the following documentation in order to improve your application:

1. Crystal Oscillator Troubleshooting Guide

2. Microcontroller Oscillator Circuit Design Considerations

Hope this material will be useful for you.

Have an excellent day :smileyhappy:

David Diaz

0 Kudos
Reply

1,726 Views
danielecortella
Contributor V

Hi,

try to put a 1Mohm resistor in parallel to the oscillator (between Extal and Xtal)

0 Kudos
Reply

1,726 Views
mjbcswitzerland
Specialist V

Hi

Make sure the high-/low gain mode is correctly set in OSC_CR

OSC_CR_HGO should be used with high loading and a feedback resistor but should not be set when there is no feedback resistor.

Regrds

Mark

Kinetis: µTasker Kinetis support

KE: µTasker FRDM-KE02Z support  / µTasker FRDM-KE02Z40M support  / µTasker FRDM-KE06Z support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos
Reply