KE02Z40 Bootloader/SDA problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KE02Z40 Bootloader/SDA problem

1,257 次查看
alexandrecapuch
Contributor I

Dear friends,
I am having problem with the BOOTLOADER and SDA of the KE02Z40M.
I'm using Windows 10 and the problem is this:
https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/

https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/


But there was no solution here, following the procedures on the page.
I need help because I have a project to complete using this uC.
I have many models of FRDM, and all are with same problems.

Thank you.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,209 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Alexandre Capucho ,

  Can you enter the bootloader mode?

  If yes, please update the bootloader version, just like this information from :

PEmicro | Experts in Embedded tools for Flash Programming and Development 

Issue: Bootloader versions 1.10 and earlier are not allowing firmware update and MSD FLASH programming on ...

Solution: Support for Windows 8/8.1, MacOS and Linux operating systems was added to Bootloader version 1.11 and MSD firmware version 1.14. Please make sure that your board is programmed with Bootloader version 1.11 or higher prior to attempting to update your OpenSDA board with a new firmware application.

Important: If you are currently running Bootloader version 1.10 or earlier, you will need to find a Windows XP or Windows 7 PC to perform this update.

Please follow these steps to find out what version of Bootloader your board is programmed with:
  1. Start your board in Bootloader mode by holding down the RESET button prior to plugging it into USB port.
  2. Open the SDA_INFO.HTM file, which will contain version numbers of Bootloader as well name and version of current OpenSDA firmware you are using. If your board is not running Bootloader version 1.11 or higher, please download the latest OpenSDA Firmware Apps from P&E website and follow instructions in corresponding documentation to update the Bootloader using the BOOTUPDATEAPP_Pemicro_v111.SDA application. Once the Bootloader is updated via BOOTUPDATEAPP, the OpenSDA board can then be upgraded to the latest combined MSD/DEBUG OpenSDA firmware 1.14 or greater.

Wish it helps you!

If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复