KE02 pinout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,382件の閲覧回数
dporada
Contributor III

I am laying out a prototype board for the MKE02Z64VQH2 (64 pin package).  I want to use both SPIs, but the reference manual seems to have an error.  SPI0_MOSI is shown on pin 31 and 59. SPI0_SCK is shown on pins 32 and 60.  I do not see a SPI1_SCK, SPI1_MOSI.

Any ideas of the correct pinout?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,182件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Donald,

  In the datasheet on the KE02 website, it lists SPI1_SCK on pin 2 and SPI1_MOSI on pin 1. I also checked the RM, and it's in there as well. Perhaps you had an older version of the materials that was missing that information.

-Anthony

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,183件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Donald,

  In the datasheet on the KE02 website, it lists SPI1_SCK on pin 2 and SPI1_MOSI on pin 1. I also checked the RM, and it's in there as well. Perhaps you had an older version of the materials that was missing that information.

-Anthony

0 件の賞賛
返信
2,182件の閲覧回数
dporada
Contributor III

Oops, you are correct.

I was looking at Alt 2 where the rest of the SPI pins were configured, not at Alt 3.

Thank you,

Don Porada

0 件の賞賛
返信