KDS v3.0 gives an error "Problems occurred during setting configuration debug for project hello_world_frdmkl03z"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS v3.0 gives an error "Problems occurred during setting configuration debug for project hello_world_frdmkl03z"

Jump to solution
2,153 Views
armaram
Contributor III

We purchased a FRDM KL03Z board and need some help with getting started with programming the board using KDS3.0.

We tried importing demos (Hello World) wsd file but get an error "Problems occurred during setting configuration debug for project hello_world_frdmkl03z"

Can anyone pls help?

Thanks,

Arvind

0 Kudos
Reply
1 Solution
1,876 Views
armaram
Contributor III

Hello Iva,

Thank you very much for the response and trying to help.

We seem to have fixed the problem. Here's what we did to resolve the problem

Step 1: Completely uninstalled the entire KDS v3.0.0 and KSDK v1.3.0 software. Also deleted previous installation folder that were not removed during un-installation.

Step 2: Disabled antivirus (we were using Total Security 360).

Step 3: Re-installed KDS v3.0.0, KDSK v1.3.0 and updated eclipse.

Step 4: Re-started PC

Invoked KDS v3.0.0 and followed the getting started guidelines. All seems ok now.

We believe it was the antivirus that was causing the problem by not allowing the tool to automatically update configurations settings.

Note: We had also observed "make not found in path" even though there was a make file visible under the debug folder.

Regards,

Arvind

View solution in original post

0 Kudos
Reply
5 Replies
1,876 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Arvind Reddy Maram,

please, what do you use for debugger? Can you show me the screenshot?

Please, take a look at

Video Link : 3282

Video Link : 3283

Thank you.

Best Regards,

Iva

0 Kudos
Reply
1,877 Views
armaram
Contributor III

Hello Iva,

Thank you very much for the response and trying to help.

We seem to have fixed the problem. Here's what we did to resolve the problem

Step 1: Completely uninstalled the entire KDS v3.0.0 and KSDK v1.3.0 software. Also deleted previous installation folder that were not removed during un-installation.

Step 2: Disabled antivirus (we were using Total Security 360).

Step 3: Re-installed KDS v3.0.0, KDSK v1.3.0 and updated eclipse.

Step 4: Re-started PC

Invoked KDS v3.0.0 and followed the getting started guidelines. All seems ok now.

We believe it was the antivirus that was causing the problem by not allowing the tool to automatically update configurations settings.

Note: We had also observed "make not found in path" even though there was a make file visible under the debug folder.

Regards,

Arvind

0 Kudos
Reply
1,876 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Arvind,

"make not found in the path" when you import .wsd file?

Best Regards,

Iva

0 Kudos
Reply
1,876 Views
armaram
Contributor III

Yes Iva, the lib files were being built without error but the hello world demo was failing with this error. That too got resolved after we did as mentioned in my previous post.

0 Kudos
Reply
1,876 Views
ivadorazinova
NXP Employee
NXP Employee

Ok Arvind,

in case of any other issue, please let us know.

Have a great day!

Best Regards,

Iva

0 Kudos
Reply