KDK for MK10DX256VLH7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDK for MK10DX256VLH7

5,344件の閲覧回数
andrewparlane2
Contributor III

We have a new custom board with a MK10DX256VLH7 on it, and I'm just getting set up to write some software. Unfortunately there doesn't seem to be a KSDK available for that package.

On https://mcuxpresso.nxp.com the only item for MK10DX256 is the MK10DX256xxx10

ksdk.png

If I download that anyway and create a new project in MCUXpresso IDE I can only choose MK10DX256xxx10 or MK12DX128xxx5 (that one comes from a different KSDK I've downloaded for a different project).

mcuxpresso1.png

If I create the project for that chip the only packages it offers me are: MK10DX256VLQ10 or MK10DX256VMD10.

mcuxpresso2.png

The datasheet for the MK10DX256VLH7 (my chip) states that the 7 means limited to 72 MHz, vs the 10 being 100 MHz. The LH is for 64 pin LQFP and the LQ / MD are both for 144 pin packages.

So does this mean I can't use the config tools and can't auto create the project via MCUXpresso IDE? I assume the drivers and everything will still work, I'll just have to manually setup the pins and clock settings? Or have I missed something?

Thanks

ラベル(1)
タグ(2)
0 件の賞賛
返信
7 返答(返信)

5,188件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi  Andrew Parlane

  Unfortunately, MK10DX256VLH7 is the old product which is not supported in the new SDK and the MCUXPresso tools.

  If you are using the 70Mhz chip, I suggest you refer to the baremetal project.

   You also can check this post:

https://community.nxp.com/message/1292192?commentID=1292192#comment-1292192 

Wish it helps you!

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

5,188件の閲覧回数
andrewparlane2
Contributor III

Hi Kerry,

Thanks for the reply.

What exactly do you mean by the baremetal project? The only software I've found for this chip so far is the stuff that comes with three application notes (AN4419SW, AN4652SW, AN4800SW) for example there are no drivers for many peripherals such as the FTM, dspi, ...

I can write all of this from scratch, but I'd prefer not to if there's an alternative.

I had a quick look through the 100MHz KSDK and there are not a huge number of references to VLQ10, 50 hits over 11 files, many of those being the different chips that come in the same package. They are mostly ifdefs surrounding quite a lot of defines for stuff like the memory map and interrupt vectors etc... How close are these two chips? Will the majority of the KSDK drivers work with my chip if I correctly set up the defines?

The config tools seems to use it's own inbuilt package definitions so I'm pretty certain I'll never be able to use those. It looks like there'sr a .zip of offline data, so I could potentially create a whole bunch of XML files that define my chip and then use those tools, but that seems like more work than it's worth. I can just set up pin muxing and configure the clock registers manually.

Are there any plans to support this (and other currently not supported chips) in the new ksdks? I thought the entire point of the MCUXpresso was to have a common interface for all of NXP's low / mid end micro controllers. I can understand not yet supporting entire families of chips, but not supporting particular packages / speed grades seems like an odd choice. Especially since this is not made clear on the product page. We would likely have not chosen this chip if we had known it wasn't supported in MCUXpresso, which is on me for not properly checking, but still is slightly disappointing.

Thanks

Andrew

0 件の賞賛
返信

5,188件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andrew Parlane,

   The baremetal code is the old code which is based on the register control, not the same format as the ongong SDK. It seems the nxp.com website remove that code package, but my side still have it, it is mainly CW and IAR project:

pastedImage_1.png

pastedImage_2.png

   I have checked the 72Mhz with our SDK department in the previous time, seems no plan to update it.

  As you know, the MCUXPresso IDE support also based on the SDK, so the MCUXpresso can't support your chip directly.

  

 If you need the baremetal code, you can create a case from the nxp.com, then I will share it with you, as I can't share it directly in the public community.

  This is the process how to create the case:

1. Open below SUPPORT site, click blue "Go to Tickets" in the middle.
http://www.nxp.com/support/support:SUPPORTHOME

2.Then you will be requested to Login, if you have no an account, please first Register with your business email.

3.After login, please "Create New Cases" button in the middle, then you can submit your question.

  Sorry for the inconvenience we bring you.

  But you still can refer to the baremetal code about the driver.

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

5,188件の閲覧回数
andrewparlane2
Contributor III

Hi Kerry, thanks for the reply.

I've created a case requesting that code #00288369.

It would also be nice to formally request that this processor is supported by the new KSDK. Given that the chip is listed as active, I don't think it's too much to ask for that it is formally supported. Please pass this request on to those who can deal with it.

Thanks

Andrew

0 件の賞賛
返信

5,188件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andrew Parlane

   Thanks for your cooperation, I already give you the 72Mhz baremetal code in the case, please check it on your side.

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

5,188件の閲覧回数
mjbcswitzerland
Specialist V

Hi Andrew

There is support for the K10DX256 70 MHz parts in the open source uTasker project (on Github) which can be used with MCUXpresso, KDS, CW, IAR, Keil, Rowley, CooCox, Greenhills, GCC make and also allows project/chip simulation with VisualStudio.

For professional requirements it is also actively supported in the uTasker Kinetis/i.MX RT developer's project which allows developing code on the K10DX256 70MHz parts that also runs on i.MX RT parts should more performance be required later, without extra development investment.

These parts are equivalent when USB is not used:

https://www.utasker.com/kinetis/TWR-K20D72M.html
https://www.utasker.com/kinetis/TEENSY_3.1.html


Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

0 件の賞賛
返信

5,187件の閲覧回数
andrewparlane2
Contributor III

Hi Mark, thanks for the reply. I'll be certain to use your code as reference. I'm hoping I can repurpose the MK10D10 KSDK, the memory map differs a bit, but I think each peripheral has essentially the same registers.

0 件の賞賛
返信