K82F erase/program flash while execute firmware in QSPI flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K82F erase/program flash while execute firmware in QSPI flash

2,256 次查看
kyleyang
Contributor IV

Hi

I built a toggle LED and erase/program external flash when button pressed.

I updated the image via KBOOT QSPI interface success and LED toggle works.

But when I pressed the button and try to erase/program QSPI flash, it will failed after program access.

Is there any idea that can help resolve this issue?

Thanks.

标签 (1)
标记 (3)
0 项奖励
回复
4 回复数

1,801 次查看
calvinday
Contributor III

I had the same problem. Remember:

1. Set FLASH_DRIVER_IS_FLASH_RESIDENT=1.

2. disable interrupts.

0 项奖励
回复

1,801 次查看
ethan_cheng
NXP Employee
NXP Employee

Hi Kyle,

QSPI controller needs to be initialized and flash operation function (ERASE and PROGRAM) need to be implemeted as RAM FUNCTION. And disable cache befor flash operation execution.

Attached the sample code for your reference.

Best regards,

Ethan

0 项奖励
回复

1,801 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Kyle Yang,

I need more details to understand your issue.

- Are you using an NXP evaluation board or custom board?

You mentioned:

But when I pressed the button and try to erase/program QSPI flash, it will failed after program access.

- Exactly what button are you pressing?

- What do you mean with "failed after program access"?

If possible please also share your LED example project.

Regards!

Jorge Gonzalez

0 项奖励
回复

1,800 次查看
kyleyang
Contributor IV

Hi Jorge Gonzalez,

I am using FRDM-K82F + KSDK2.1 for QSPI test based on the "qspi_polling_transfer".

I attached my project code and BD file for your reference.

I move the QSPI W/R related code to access at RAM.

Now ERASE is working, but write will not functional correct.

0 项奖励
回复