K82 : wakeup from LLS3 mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K82 : wakeup from LLS3 mode

799 次查看
EugeneHiihtaja
Senior Contributor I

Hello !

When MCU wake up from LLS3 mode , some LLWU interrupts should be cleaned as it mentioned in example.

But what about waiting some time for clock stabilisation ?

power_user_config_t targetConfig;
targetConfig.enableLpoClock = true;
targetConfig.mode = kAPP_PowerModeLls;
PM_PowerModeSwitch(&targetConfig, NULL);
//
// ... LLS3 ....
//
// Wakeup -> continue execution
//
// LLS3 –> RUN — 6.3 μs, see specification for exact clocks and etc.
//

/* Wait for PLL lock. MCG in PEE mode in RUN. */
while (!(kMCG_Pll0LockFlag & CLOCK_GetStatusFlags()))
{
}
CLOCK_SetPeeMode();

/* Power mode change. */
SMC_SetPowerModeRun(SMC); // No need ?
while (kSMC_PowerStateRun != SMC_GetPowerModeState(SMC))
{
}

Does this red color part is right one ?

Regards,

Eugene

0 项奖励
回复
1 回复

712 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Eugene,

If previous mode is VLPR and you want going to RUN mode, you should call this function. Otherwise, this function have no impact to system.

Regards,

Jing

0 项奖励
回复