K82: performance of hw random generator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K82: performance of hw random generator

3,834件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

Do I measure right and performance of TRNG random generator is about 100 bytes per seconds ?

Bus clock - 60 Mhz.

Regards,

Eugene

0 件の賞賛
返信
6 返答(返信)

3,686件の閲覧回数
mjbcswitzerland
Specialist V

Eugene

The True Random Number Generator is a very high quality entropy source but takes a long time to complete its operation. I think that idea is to use it to seed a Pseudo Random Number Generator for subsequent use (which will be implemented in SW) and not to use it to generate each random number.

Regards

Mark

0 件の賞賛
返信

3,686件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi Mark !

Yes, it is typical technique to use it, but it would be nice to know if my digits are correct for be sure if everything configured properly.

Regards,

Eugene

3,686件の閲覧回数
mjbcswitzerland
Specialist V

Eugene

As you will know, the TRNG generates 16 long words of entropy each time it is used ( (64 bytes).

When I test this it takes typically between 590ms and 650ms, which would give approx. 10ms per byte, which corresponds to your 100bytes/s (or 10ms per byte).

I use this configuration on the K82F:

    POWER_UP_ATOMIC(3, TRNG0);                                           // power up TRNG0
    TRNG0_MCTL = (TRNG_MCTL_PRGM | TRNG_MCTL_RST_DEF);                   // ensure we are in programming mode with defaults set
    TRNG0_FRQMIN = 0;
    TRNG0_FRQMAX = 0x03ffff;                                             // the default maximum value is too low and causes a frequency count failure if not increased
    TRNG0_SDCTL = ((1600 << 16) | (2500));                               // entropy delay and sample size reduced to half of default
    TRNG0_MCTL = (TRNG_MCTL_PRGM_RUN | TRNG_MCTL_SAMP_MODE_VON_NEUMANN | TRNG_MCTL_TRNG_ACC | TRNG_MCTL_OSC_DIV_1); // set to run mode with TRNG access
‍‍‍‍‍‍

Regards

Mark

3,686件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi Mark !

Thank you !

Pseudo random generator  from standart C library rand() utilize some global buffers what cause problem to run code with User privileges.

Better to allocate this buffer from RTOS Task stack and use after that in context of this task.

Do you know any public implementation of pseudo random generator what available with source code ?

Regards,

Eugene

0 件の賞賛
返信

3,686件の閲覧回数
mjbcswitzerland
Specialist V

Eugene

Try mbedTLS as reference.

Simplified:

They use a 16 byte long counter which is seeded from an entropy source [which can bet quite complicated if there is no good source] (TRNG would be used for this since it is an excellent source).
It then performs an AES_ECB (AES256) encryption to generate 16 bytes of output and increments the 16 byte before each use. The 16 bytes of output are used as random numbers.


It sometimes re-seeds itself (based on elapsed time or a number of utilisations).

Since the K80 can do AES256 in HW this algorithm looks suitable.

Regards

Mark

0 件の賞賛
返信

3,686件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi Mark !

Thank you !

Regards,

Eugene

0 件の賞賛
返信