K82 : MCUExpresso disable heap usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K82 : MCUExpresso disable heap usage

2,603件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

I use latest MCU Expresso and SDK for develop firmware for K82.

How-to completely disable heap usage and be sure if malloc/free is not called suddenly somewhere ?

I have set HeapSize =0 in Linker file and set trap for malloc/free in linker options.

But looks like heap is used somewhere in any case.

-Xlinker --wrap=malloc -Xlinker --wrap=free -Xlinker --wrap=calloc

But linker report :

c:/nxp/mcuxpressoide_10.3.0_2200/ide/plugins/com.nxp.mcuxpresso.tools.win32_10.3.0.201811011841/tools/bin/../lib/gcc/arm-none-eabi/7.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/fpv4-sp/hard\libcr_c.a(fpprintf.o): In function `printf':
fpprintf.c:(.text.printf+0x1e): undefined reference to `__wrap_malloc'
fpprintf.c:(.text.printf+0x3e): undefined reference to `__wrap_free'


c:/nxp/mcuxpressoide_10.3.0_2200/ide/plugins/com.nxp.mcuxpresso.tools.win32_10.3.0.201811011841/tools/bin/../lib/gcc/arm-none-eabi/7.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/fpv4-sp/hard\libcr_c.a(fclose.o): In function `fclose':
fclose.c:(.text.fclose+0x24): undefined reference to `__wrap_free'

How-to disable heap in MCUExpresso and K82 in correct way ?

Regards,

Eugene

0 件の賞賛
返信
4 返答(返信)

2,367件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You don't have much control what the GNU library does: internally it can use malloc() for things like printf() or file I/O. Another reason not to use the prinf() of the library. But what you can do is to disable at least some of it with selecting a 'none' or no-host' library variant:

pastedImage_1.png

The other way is that you overwrite the malloc() and free() functions with your own version to trap all usage of it.

I hope this helps,

Erich

0 件の賞賛
返信

2,367件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi Erich !

I have MPU enabled environment  and any extra memory accesses to unknown area cause faults.

In linker file I set nohost version already 

/* Redlib Nohost */
GROUP(libcr_nohost.a libcr_c.a libcr_eabihelpers.a)

And in project settings it show nohost-nf like you recommend.

printf() is not used for sure but snprintf() is used for cook formatted strings.

Also FreeRTOS in some debug places use sprintf() functions.

Do you have idea why is latest MCUXpressoIDE_10.3.0_2200 is so slow in case of compilation ?

Previos version is fly on my computer, but current one need 5 min for compile project, even before it was 1 min.

Regards,

Eugene

0 件の賞賛
返信

2,367件の閲覧回数
bobpaddock
Senior Contributor IV

Having directories in the path that do not exist can slow GCC to a crawl at times.

printf() and  snprintf() will likely call the same underlying print library.

Random tip that came to mind when reading your message, make sure all the stack are always aligned to an eight byte (long long) boundary when initialized.  Generally this happens by default by pointing at the end of RAM.

0 件の賞賛
返信

2,367件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi Erich !

One more experiment. I have taken printf-stdarg.c implementation from Freertos examples and references to malloc/calloc are vanish.

But free is still in use somewhere c:/nxp/mcuxpressoide_10.3.0_2200/ide/plugins/com.nxp.mcuxpresso.tools.win32_10.3.0.201811011841/tools/bin/../lib/gcc/arm-none-eabi/7.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/fpv4-sp/hard\libcr_c.a(fclose.o): In function `fclose':
fclose.c:(.text.fclose+0x24): undefined reference to `__wrap_free'
collect2.exe: error: ld returned 1 exit status

fclose() is actively used in mbedTLS  common code but for K82 it is excluded in configuration by using #ifdef flags.

May be linker is not willing so strip it or this call exists in other call function ?

At list active code dosn't have reference to it.

Any ideas ?

Regards,

Eugene

0 件の賞賛
返信