K82: LLWU_SetPinFilterMode() API

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K82: LLWU_SetPinFilterMode() API

1,153 Views
EugeneHiihtaja
Senior Contributor I

Hello !

Could you clarify a bit what LLWU filter means ?

As input it has structure llwu_external_pin_filter_mode_t

what has parameter

typedef enum _llwu_pin_filter_mode
{
kLLWU_PinFilterDisable = 0U, /*!< Filter disabled. */
kLLWU_PinFilterRisingEdge = 1U, /*!< Filter positive edge detection.*/
kLLWU_PinFilterFallingEdge = 2U, /*!< Filter negative edge detection.*/
kLLWU_PinFilterAnyEdge = 3U /*!< Filter any edge detection. */
} llwu_pin_filter_mode_t;

But edge detection is set by LLWU_SetExternalWakeupPinMode() API.

in RM , chpter 19.5 I can see

"

The LLWU implements optional 3-cycle glitch filters, based on the LPO clock. A
detected external pin is required to remain asserted until the enabled glitch filter times
out. Additional latency of up to 2 cycles is due to synchronization, which results in a total
of up to 5 cycles of delay before the detect circuit alerts the system to the wakeup or reset
event when the filter function is enabled. wakeup detect filters are available for selected
external pins. Glitch filtering is not provided on the internal modules.

"

How setup proper filter for LLWU pin ? I use LLS3 low power mode if it any difference with other low power  modes.

Regards,

Eugene

0 Kudos
Reply
1 Reply

1,065 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Eugene,

If kLLWU_ExternalPinRisingEdge is selected, then you should configure kLLWU_PinFilterRisingEdge.

Notice VLLS0 mode:

filters will be bypassed during VLLS0.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply