K82 : FLASH_PflashSetProtection & FLASH_PflashGetProtection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K82 : FLASH_PflashSetProtection & FLASH_PflashGetProtection

1,607 次查看
EugeneHiihtaja
Senior Contributor I

Hello !

Can it be so that those API is not work properly ?

"

if (config->ftfxConfig[0].flashDesc.feature.hasProtControl)
{
if (config->ftfxConfig[0].flashDesc.feature.ProtRegBits >= 32)
{
*kFPROTL = protectStatus->protl;
if (protectStatus->protl != *kFPROTL)
{
return kStatus_FTFx_CommandFailure;
}
}

"

ProtRegBits need to be set to 32 but no any code in SDK is not exists to do it ? It has value 0 ?

It should be set here FLASH_Init(...) but this is not visible.

Rregards,

Eugene

0 项奖励
回复
3 回复数

1,516 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eugene,

    Actually, FLASH_PflashSetProtection API is used to set the protection bit, write the Program Flash Protection Registers

pastedImage_18.png

It is 4Bytes, just 32bit.

ProtRegBits can be set by yourself in the code, you totally can define it.

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,516 次查看
EugeneHiihtaja
Senior Contributor I

Hi Kerry !

Yes, I have modified it by myself. But it is clear defect in SDK and have sense to improve it at some point.

Regards,

Eugene

0 项奖励
回复

1,516 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eugene,

   Thank you for your updated information.

   This variable normally need to be configured in the main code before you call the according API, so this point is not the SDK bug.

   Any way, next time, when the SDK do the improvement, I will suggest it.

 


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复