K82: ARM errata 838869 and SysTick handler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K82: ARM errata 838869 and SysTick handler

2,410 Views
EugeneHiihtaja
Senior Contributor I

Hi !

 

I can see _DSB() entry  in almost all interrupt handlers for fix errata case.

 

But not in TickTimerHandler in FreeRTOS port.c:

 

void xPortSysTickHandler(void)
{
   uint32_t ulDummy;

   ulDummy = portSET_INTERRUPT_MASK_FROM_ISR();
   {
   /* Increment the RTOS tick. */
      if (xTaskIncrementTick() != pdFALSE)
      {
         /* Pend a context switch. */
         portNVIC_INT_CTRL_REG = portNVIC_PENDSVSET_BIT;
      }
   }
   portCLEAR_INTERRUPT_MASK_FROM_ISR(ulDummy);

 

// ???

}

 

Even if I unroll all macros, _DSB is not visible.

Or errata is not effect special handlers ?

 

By the way, do you have idea when new SDK will be released  with new FreeRTOS 10.1.0 for K82 ?

Regards,

Eugene

0 Kudos
Reply
1 Reply

1,711 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Eugene,

DSB is used before ISR return only if ISR's last operation is accessing peripheral registers.

Regarding your other question, we don't have a date for the release of the SDK with the new version of FreeRTOS. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply