K81 blhost spi error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K81 blhost spi error

1,285 Views
kaustubhkulkarn
Contributor I

Hello,

I am working on the K81. I am using blhost with spi (run mode with 4Mbps) to write .sb file to the QSPI memory. But I am getting following error.

Inject command 'receive-sb-file'
Preparing to send 345760 (0x546a0) bytes to the target.
Successful generic response to command 'receive-sb-file'
(1/1)0%Error: read_start_byte() timeout after 10.037 seconds
Data phase write aborted by status 0x5 kStatus_Timeout
Error: read_start_byte() timeout after 10.025 seconds
Response status = 10004 (0x2714) No response packet from target device.
Wrote 672 of 345760 bytes.

Could you please help me with this.

Thank you.

0 Kudos
Reply
1 Reply

1,212 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

I'm not sure if you connect your system correctly. Please review <Kinetis blhost User's Guide.pdf> for detail. In Appendix C, it describes how to download code by blhost if you want to use SPI.

Regards,

Jing

0 Kudos
Reply