I want to use uart0 for ISO 7816
SIM power is connected to GPIO
SIM reset is connected to GPIO
SIM clock is connected to FTM0_3
SIM Data is connected to UART0 TX
How to initialize uart0 and FTM0_3.
and how to get ATR information.
please help me
Solved! Go to Solution.
Hi Stephanos,
The attachment includes all the source files for this demo, you may run the "make_new_project.exe" in the folder of "KINETIS_120MHZ_SC\build\iar", and create a project named as "iso7816_demo", and then copy and replace all the files in the folder of "KINETIS_120MHZ_SC\src\projects\iso7816_demo" with the attached one.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Stephanos Choi,
Please kindly refer to the attached ISO7816 demo for details. It is based on TWR-K70F120M.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have KINETIS_120MHZ_SC but cannot find the demo.
where is it in KINETIS_120MHZ_SC?
I wrote that demo based on KINETIS_120MHZ_SC, so it is not in the released version.. Please kindly refer to the attached KINETIS_120MHZ_SC.7z.zip for details.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Kan
But I cannot down load the file, it is displayed like"Security policy violation detected. The file has been removed."
Please send me the file to e-mail ( [email protected] ).
Have a nice day.
Stephanos
Hi Stephanos,
The attachment includes all the source files for this demo, you may run the "make_new_project.exe" in the folder of "KINETIS_120MHZ_SC\build\iar", and create a project named as "iso7816_demo", and then copy and replace all the files in the folder of "KINETIS_120MHZ_SC\src\projects\iso7816_demo" with the attached one.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------