K70 SysTick Clock Source Bit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K70 SysTick Clock Source Bit

跳至解决方案
2,570 次查看
pmcl
Contributor I

Hi All,

I'm using the K70 SysTick Timer and referred to the K70P256M150SF3EM manual, section 3.2.1.2 on page 85 which says that the CLKSOURCE bit in the SysTick Control and Status Register is always set to select the core clock. However, if I have this line in KDS3.0.0:

  SYST_CSR = (SysTick_CSR_ENABLE_MASK | SysTick_CSR_TICKINT_MASK);

it does not generate an interrupt - which means SysTick is not ticking. If I use:

  SYST_CSR = (SysTick_CSR_ENABLE_MASK | SysTick_CSR_TICKINT_MASK | SysTick_CSR_CLKSOURCE_MASK);

I do get an interrupt.

I thought the value of CLKSOURCE was always set and not writable, so the first bit of code is all that is needed?

Since that code writes a 0 to the CLKSOURCE bit, does that mean it is writable, and therefore not always "set"?

Thanks!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,235 次查看
mjbcswitzerland
Specialist V

Peter

The core clock is selected by default but there is nothing stopping you writing it to 0 and thus disabling it.

See also ARM Information Center

Regards

Mark

Kinetis: µTasker Kinetis support

K70: µTasker Kinetis TWR-K70F120M support  / µTasker EMCRAFT K70F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,236 次查看
mjbcswitzerland
Specialist V

Peter

The core clock is selected by default but there is nothing stopping you writing it to 0 and thus disabling it.

See also ARM Information Center

Regards

Mark

Kinetis: µTasker Kinetis support

K70: µTasker Kinetis TWR-K70F120M support  / µTasker EMCRAFT K70F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复
2,235 次查看
pmcl
Contributor I

Thanks Mark.

I was relying on the Freescale documentation and didn't go "down a level" to the ARM documentation, which makes it clear that the CSR register is set to 0x000_0004 coming out of reset if the alternate reference clock is not present.

I think Freescale should change the line:

"- The CLKSOURCE bit in SysTick Control and Status register is always set to select the core clock."

so that it says "initialised to 1 after a reset".

0 项奖励
回复