K70 SDK where to download?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K70 SDK where to download?

1,128 Views
gustavoparlanti
Contributor I

I develop my own K70 SOM hardware and I want to download the K70 SDK and it is not available where I can get it?

Labels (1)
0 Kudos
Reply
2 Replies

975 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Gustavo Parlanti,

Unfortunately, at the moment there is no plan to support this part number with SDK libraries.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

975 Views
mjbcswitzerland
Specialist V

Hi Gustavo

I believe there is no more NXP support for K70 in newer tool chains.

There are still links to older MQX versions around though.

It is however still supported in the uTasker project with all new tool-chains, which is also available as free open source, where you can simply add a simulation model for your SOM - https://github.com/uTasker/uTasker-Kinetis

Regards

Mark

0 Kudos
Reply