K70 SAI transmitter not send data :(

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K70 SAI transmitter not send data :(

3,497 次查看
adampitak
Contributor III

Hello

I m trying configure SAI0 as regular transmitter, everything working fine but on output I2S0_TXD0 I have no data Smiley Sad

MCLK, I2S0_TX_FS, I2S0_TX_BCLK work good.

I push data into I2S0_TDR0 and in interrupt from SAI check FRF bit from TCSR register

Thank You for answers and help.

here is my config:

SIM_SCGC6 |= SIM_SCGC6_SAI0_MASK; // enable I2S module

  

    I2S0_TCR1 |= I2S_TCR1_TFW(3); //watermark level

  

    I2S0_TCR2 |= I2S_TCR2_MSEL(1) | //MCLK select from CLKGEN
I2S_TCR2_BCD_MASK | // bit clock direction
I2S_TCR2_DIV(0); // from MCLK divider to BCLK (max 256)

  

    I2S0_TCR3 |= I2S_TCR3_TCE(2); // Transmit channel enable; TDR0=2; TDR1=1 ????

  

    I2S0_TCR4 |=  I2S_TCR4_FRSZ(1) | //number of words in frame
I2S_TCR4_SYWD(31) | //number bits in frame
I2S_TCR4_MF_MASK | //frame sync polarity MSB/LSB first
I2S_TCR4_FSE_MASK | //Frame sync early: log.0 Justified, log.1 I2S
I2S_TCR4_FSD_MASK; //frame sync direction

  

    I2S0_TCR5 |= I2S_TCR5_WNW(31) | // number of bits in next word
I2S_TCR5_W0W(31) | // number of bits in first word
I2S_TCR5_FBT(31); //first bit shiffed

  

    I2S0_MCR |= I2S_MCR_MOE_MASK | //MCLK generated internally
I2S_MCR_MICS(3); //MCLK input clock select from PLL=120 MHz

  

    I2S0_MDR |= I2S_MDR_DIVIDE(999)| //2722 (fract + 1)
I2S_MDR_FRACT(6); // MCLKout = MCLKin * -------------
// (divide +1)

  

    PORTE_PCR6 |= PORT_PCR_MUX(0x04); // configure port for MCLK output
    PORTE_PCR10 |= PORT_PCR_MUX(0x04); // configure port for I2S0_TXD0
    PORTE_PCR11 |= PORT_PCR_MUX(0x04); // configure port for I2S0_TX_FS
    PORTE_PCR12 |= PORT_PCR_MUX(0x04); // configure port for I2S0_TX_BCLK

  

    I2S0_TCSR |= I2S_TCSR_TE_MASK | //enable transmitter
I2S_TCSR_STOPE_MASK | //stop enable
I2S_TCSR_FR_MASK | //reset fifo pointers
I2S_TCSR_FRIE_MASK ; //enable interrupt from watermark
标签 (1)
10 回复数

2,661 次查看
adampitak
Contributor III
Problem is solved:
1. fill configuration register and fill FIFO
2. then set to "1" Transmitter enable:  I2S0_TCSR |= I2S_TCSR_TE_MASK
NOT IN REVERSE !!!!

by the way... in manual nothing say this thing!!

by the way... in TCR3 bits TCE: 16-th bit represents FIFO "0" (TDR0,TFR0)

                                               17-th bit represents FIFO "1" (TDR1,TFR1)

2,661 次查看
gerardovaldovin
Contributor I

Hello Adam.

Right now I'm having the same problems you had with SAI. I was wondering if you can send me that part of code. I really will appreciate it.

Thanks in advance.

0 项奖励
回复

2,661 次查看
adampitak
Contributor III

Or is there somebody who have example SAI (I2S) as transmitter for K70 ???

Thank you so much.

0 项奖励
回复

2,661 次查看
egoodii
Senior Contributor III

I can only suggest my I2S/DMA example in community.freescale.com/thread/114450.  It was written for version 1 silicon, so if you have the 'version 2' SAI block in your chip, I'm afraid there will be differences.

0 项奖励
回复

2,661 次查看
adampitak
Contributor III

Hi thank you for response, but Your code looks like for K60... it is different I2S interface :smileysad:

Adam

0 项奖励
回复

2,661 次查看
egoodii
Senior Contributor III

Sorry -- that was my concern about the 'Version 1' vs 'Version 2' silicon.

0 项奖励
回复

2,661 次查看
adampitak
Contributor III

But these can help, I have "Device revision number: 0" of K70FN1M0VMJ12, maybe itis old

0 项奖励
回复

2,661 次查看
egoodii
Senior Contributor III

Sorry again, 'version' can be a tricky thing to pin down.  I refer specifically to the differences outlined in AN4445.pdf.  I would say your original statement is correct, in that my firmware was designed for the SSI, and newer parts have this SAI which is 'similar' but to be sure differs in some very serious ways.  Sorry I can't be of more help.

0 项奖励
回复

2,661 次查看
egoodii
Senior Contributor III

Just as a 'simple statement' totally unrelated to the exact details of the SAI --- I see most of your register controls are set with 'OR-equals' operators, and I would certainly be more inclined to directly set the full contents of many of these control registers, most especially the PORT_PCR controls.

0 项奖励
回复

2,661 次查看
adampitak
Contributor III

Hi, Thank you for your reply, now I understand what you meant (difference between SSI and SAI),

but nothing solved my problem :smileycry:

I tried PORTE_PCR10 = PORT_PCR_MUX(0x04); and all configure register with "="

Can be problem that I´m using MQX? by the way, MQX never touch PTE10

0 项奖励
回复