K70 - LCD - max portrait resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K70 - LCD - max portrait resolution

ソリューションへジャンプ
2,888件の閲覧回数
arnaud
Contributor I

Hello,

What is the maximum resolution for a portrait TFT driven by a K70 (MK70FN1M0VMJ15) ?

The K70 Sub-Family Reference Manual indicates : Maximum resolution of 800 × 600.

but... the document "Configuring the K70 LCDC Using TWR-LCD-RGB" shows (p.8) an example with a Active frame height of 800.

I would like to interface a portrait LCD 480 x 800, would it be possible ??

LCDC_LSR : XMAX = 480/16 = 30

LCDC_LSR : YMAX = 800

Thank you for any help !

Arnaud

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,660件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Arnaud,

  Yes, a 480x800 LCD is possible. In fact during early development of that was the original resolution of the TWR-LCD-RGB, so I can confirm that resolution will definitely work. The 800x600 number is based on bandwidth requirements. The actual max for any one direction is determined by the LCDC_LSR XMAX and YMAX fields.

Anthony

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,661件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Arnaud,

  Yes, a 480x800 LCD is possible. In fact during early development of that was the original resolution of the TWR-LCD-RGB, so I can confirm that resolution will definitely work. The 800x600 number is based on bandwidth requirements. The actual max for any one direction is determined by the LCDC_LSR XMAX and YMAX fields.

Anthony

0 件の賞賛
返信
2,660件の閲覧回数
arnaud
Contributor I

Hi Anthony,

Thank you !

Arnaud.

0 件の賞賛
返信