K70, Keil and SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K70, Keil and SDK

1,542 Views
larskollros
Contributor I

Hi,

I try to get some sample project for the K70 and the LCD (which this mcu should be made for), but it seems to be all a mess.

The SDK for this controller is nearly empty.

The support for KEIL is also nearly not existent.

at the moment a have a crash after this line (originally in the sdram.c)

     * (vuint32 *)(0x400Ae1ac) = 0x01030203;

DDR_CR00 = 0x00000400;// DDRCLS = 4 is reserved??

I even can`t throw it out of the window, beause i cant open my window :smileysad:

can anyone help me?

will there be an improved support for the K70 and Keil soon?

Labels (1)
0 Kudos
Reply
1 Reply

1,358 Views
apanecatl
Senior Contributor II

I am afraid the K70 LCDC projects/demos were only made for CodeWarrior and IAR, those projects might not be fully supported in Keil for a time.

0 Kudos
Reply