K70 JTAG interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K70 JTAG interface

3,061件の閲覧回数
thefinalset
Contributor I

Hi all, I am designing a device for a school project using a member of Kinetis K70 family and I am having problems with the JTAG part of the schematic.  I am not sure where to connect what, as the PE Micro JTAG interface I have is 20 pin for the Kinetis.  Could someone please provide me with the schematic for the JTAG inteface or point me to it?  Thanks much! 

0 件の賞賛
返信
3 返答(返信)

2,303件の閲覧回数
iafg
Contributor IV
Look for the schematics at www.Freescale.com /tower
0 件の賞賛
返信

2,303件の閲覧回数
thefinalset
Contributor I

Thanks iafg!!

 

I got the schematic for the TWR-K70F120M and the user manual has the pinout.  I on;y have one concern remaning, the pinout for the JTAG connector is different than the one I found for ARM processors here:  http://www.jtagtest.com/pinouts/arm20  

 

which do I trust? 

0 件の賞賛
返信

2,303件の閲覧回数
iafg
Contributor IV

The "20 pin" interface you show is the older 0.100" spaced one.

The "19 pin interface is what is used on Kinetis. It's really a 20 pin with one pin removed.

The 19 pin is 0.050" spaced pins and is much smaller. You will need an adapter if you are plugging into the older "BIG" 20 pin JTAG

 

In addition to this there is a smaller 9 pin version.

You can see them here:

http://www.segger.com/jlink-adapters.html

look up

  • J-Link 19-pin Cortex-M Adapter
  • J-Link 9-pin Cortex-M Adapter

 

0 件の賞賛
返信