K70 Ethernet inperrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K70 Ethernet inperrupt

1,365 次查看
stephanoschoi
Contributor II

I'm using TWR-K70 and TWR-SER.

I'm initialize port first..

and then

MK70_SIM_REGISTER_SCGC2 |= MK70_SIM_SCGC2_ENET1_MASK;    // Clock On

HardwareEthernet.SystemEndian = memory_get_system_endian();
hardware_ethernet_reset();    // Reset
hardware_ethernet_disable();   // Disable Block
MK70_ENET_REGISTER_EIMR = 0;   // Mask all FEC interrupts
MK70_ENET_REGISTER_EIR = 0xFFFFFFFF; // Clear all FEC interrupt events
// MK70_ENET_REGISTER_EIR = MK70_ENET_EIR_TS_TIMER_MASK
//         | MK70_ENET_EIR_TS_AVAIL_MASK
//         | MK70_ENET_EIR_WAKEUP_MASK
//         | MK70_ENET_EIR_PLR_MASK
//         | MK70_ENET_EIR_UN_MASK
//         | MK70_ENET_EIR_RL_MASK
//         | MK70_ENET_EIR_LC_MASK
//         | MK70_ENET_EIR_EBERR_MASK
//         | MK70_ENET_EIR_MII_MASK
//         | MK70_ENET_EIR_RXB_MASK
//         | MK70_ENET_EIR_RXF_MASK
//         | MK70_ENET_EIR_TXB_MASK
//         | MK70_ENET_EIR_TXF_MASK
//         | MK70_ENET_EIR_GRA_MASK
//         | MK70_ENET_EIR_BABT_MASK
//         | MK70_ENET_EIR_BABR_MASK;

// Clear MAC address
MK70_ENET_REGISTER_PALR = 0;
MK70_ENET_REGISTER_PAUR = 0;
// Clear the Individual Address Hash registers
MK70_ENET_REGISTER_IALR = 0; // Set unicast address hash table
MK70_ENET_REGISTER_IAUR = 0; // Set unicast address hash table
// Clear the Group Address Hash registers
MK70_ENET_REGISTER_GALR = 0; // Set multicast address hash table
MK70_ENET_REGISTER_GAUR = 0; // Set multicast address hash table

// Set interrupt mask
// Enable Transmit Frame Interrupt, Receive Frame Interrupt, BUS Error Interrupt
// MK70_ENET_REGISTER_EIMR = (MK70_ENET_EIMR_TXF_MASK | MK70_ENET_EIMR_RXF_MASK | MK70_ENET_EIMR_EBERR_MASK);
MK70_ENET_REGISTER_EIMR = 0
       | MK70_ENET_EIMR_BABR_MASK
//       | MK70_ENET_EIMR_BABT_MASK
//       | MK70_ENET_EIMR_GRA_MASK
       | MK70_ENET_EIMR_TXF_MASK
//       | MK70_ENET_EIMR_TXB_MASK
       | MK70_ENET_EIMR_RXF_MASK
       | MK70_ENET_EIMR_RXB_MASK
//       | MK70_ENET_EIMR_MII_MASK
       | MK70_ENET_EIMR_EBERR_MASK
//       | MK70_ENET_EIMR_LC_MASK
//       | MK70_ENET_EIMR_RL_MASK
//       | MK70_ENET_EIMR_UN_MASK
       | MK70_ENET_EIMR_PLR_MASK
//       | MK70_ENET_EIMR_WAKEUP_MASK
//       | MK70_ENET_EIMR_TS_AVAIL_MASK
//       | MK70_ENET_EIMR_TS_TIMER_MASK
       ;


// Set PAUSE frame duration
MK70_ENET_REGISTER_OPD = (MK70_ENET_OPD_OPCODE(0x00) | MK70_ENET_OPD_PAUSE_DUR(0x00));
// Set transmit control register
MK70_ENET_REGISTER_TCR = (MK70_ENET_TCR_ADDSEL(0x00) | MK70_ENET_TCR_FDEN_MASK); // Enable Full Duplex
// Set transmit accelerator function configuration register
MK70_ENET_REGISTER_TACC = 0x00000000; // disable insert protocol checksum, IP header checksum, and TX fifo shift

// Set receive control register
MK70_ENET_REGISTER_RCR = MK70_ENET_RCR_MII_MODE_MASK /*always*/
       | MK70_ENET_RCR_RMII_MODE_MASK /*We using RMII mode*/
       | MK70_ENET_RCR_MAX_FL(ETHERNET_FRAME_MAXIMUM_LENGTH) /*check frame length*/
       | MK70_ENET_RCR_FCE_MASK; /*Flow control enable*/
//       | MK70_ENET_RCR_CRCFWD_MASK; /*no CRC pad required*/
// Set receive accelerator function configuration register
MK70_ENET_REGISTER_RACC = 0x00000000; // not discard Error frame, wrong checksum frame and IP header checksum error frame, pad not removed, and RX fifo shift

// Set transmit inter-packet gap
MK70_ENET_REGISTER_TIPG = MK70_ENET_TIPG_IPG(0x08/*8~27*/);
// Set frame truncation length
MK70_ENET_REGISTER_FTRL = MK70_ENET_FTRL_TRUNC_FL((((ETHERNET_FRAME_MAXIMUM_LENGTH/*1518*/ % 64) != 0) ? (((ETHERNET_FRAME_MAXIMUM_LENGTH/*1518*/ / 64) + 1) * 64) : ETHERNET_FRAME_MAXIMUM_LENGTH));
// Set transmit FIFO watermark
MK70_ENET_REGISTER_TFWR = (MK70_ENET_TFWR_STRFWD_MASK | MK70_ENET_TFWR_TFWR(0x00)); // Store & forward enable transmit FOFO write 64 bytes written
// Set transmit FIFO section empty threshold
MK70_ENET_REGISTER_TSEM = MK70_ENET_TSEM_TX_SECTION_EMPTY(0x00);
// Set transmit FIFO almost empty threshold
MK70_ENET_REGISTER_TAEM = MK70_ENET_TAEM_TX_ALMOST_EMPTY(0x08);
// Set transmit FIFO almost full threshold
MK70_ENET_REGISTER_TAFL = MK70_ENET_TAFL_TX_ALMOST_FULL(0x08);
// Set receive FIFO section full threshold
MK70_ENET_REGISTER_RSFL = MK70_ENET_RSFL_RX_SECTION_FULL(0x00);
// Set receive FIFO section empty threshold
MK70_ENET_REGISTER_RSEM = MK70_ENET_RSEM_RX_SECTION_EMPTY(0x00);
// Set receive FIFO almost empty threshold
MK70_ENET_REGISTER_RAEM = MK70_ENET_RAEM_RX_ALMOST_EMPTY(0x08);
// Set receive FIFO almost full threshold
MK70_ENET_REGISTER_RAFL = MK70_ENET_RAFL_RX_ALMOST_FULL(0x08);
// Set MII speed control register
hardware_ethernet_mii_initialize();
// Clear statistic counters
hardware_ethernet_clear_statistics();
// Set default MAC address
hardware_ethernet_set_mac_address(HardwareEthernet.pMAC);
// Buffer Initialize
hardware_ethernet_buffer_initialize();

hardware_interrupt_set_prority(INTERRUPT_NUMBER_ENET_TRANSMIT, INTERRUPT_PRIORITY_6);
hardware_interrupt_set_prority(INTERRUPT_NUMBER_ENET_RECEIVE, INTERRUPT_PRIORITY_6);
hardware_interrupt_set_prority(INTERRUPT_NUMBER_ENET_ERROR, INTERRUPT_PRIORITY_6);

hardware_ethernet_phy_initialize();
hardware_ethernet_enable();

hardware_interrupt_enable(INTERRUPT_NUMBER_ENET_TRANSMIT);
hardware_interrupt_enable(INTERRUPT_NUMBER_ENET_RECEIVE);
hardware_interrupt_enable(INTERRUPT_NUMBER_ENET_ERROR);

then... not occur interrupt.

when polling  'MK70_ENET_REGISTER_EIR'

TX frame interrupt bit is set when transmit

TX frame interrupt bit is set when receive

but not occur interrupt.

any one help me?

标签 (1)
0 项奖励
回复
3 回复数

1,121 次查看
mjbcswitzerland
Specialist V

Hi

Have interrupts been enabled in the Cortex core, as well as in the EMAC?

Regards

Mark

0 项奖励
回复

1,121 次查看
stephanoschoi
Contributor II

followings are display a enabling core interrupt


hardware_interrupt_enable(INTERRUPT_NUMBER_ENET_TRANSMIT);
hardware_interrupt_enable(INTERRUPT_NUMBER_ENET_RECEIVE);

hardware_interrupt_enable(INTERRUPT_NUMBER_ENET_ERROR);


........................


int hardware_interrupt_enable(qInterruptNumber InterruptNumber)

{

return  core_nvic_interrupt_enable((uint32_t)InterruptNumber);

}


int core_nvic_interrupt_enable(uint32_t InterruptNumber)

{

if(InterruptNumber < 240)

{

  if((CORTEX_M4_PERIPHERAL_REGISTER_NVIC_ISER(InterruptNumber >> 5) & (1 << (InterruptNumber & 0x0000001F))) == 0)

  {

   CORTEX_M4_PERIPHERAL_REGISTER_NVIC_ICER(InterruptNumber >> 5) |= (1 << (InterruptNumber & 0x0000001F));

   CORTEX_M4_PERIPHERAL_REGISTER_NVIC_ISER(InterruptNumber >> 5) |= (1 << (InterruptNumber & 0x0000001F));

   return 0;

  }

  return 2;

}

return 1;

}


#define CORTEX_M4_PERIPHERAL_REGISTER_NVIC_ISER(Index) (CORTEX_M4_PERIPHERALS_POINTER->NVIC_ISER[Index])

#define CORTEX_M4_PERIPHERAL_REGISTER_NVIC_ICER(Index) (CORTEX_M4_PERIPHERALS_POINTER->NVIC_ICER[Index])




0 项奖励
回复

1,121 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Stephanos,

is it necessary for you to use the Ethernet module in a bareboard project? Have you thought on using a stack? This is most common as it provides many services. May I ask what is your application? We provide RTCS (Real Time Communications Suite) in MQX, this stack provides TCP/IP support and many other protocols, this could be useful for you. You can take a look in www.freescale.com/mqx

Best regards,

Carlos

0 项奖励
回复