K70 DSP benchmark test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K70 DSP benchmark test

8,313 Views
poul-erikhansen
Contributor II

I have made the following benchmark test on a TWR-K70F120M board.

I have used the ARM CMSIS DSP library.

I have used the IAR Embedded Workbench 7.20.

 

Used if you can Poul-Erik.

 

 

freescale TWR-MK70F120M: ARM cortex M4 120 MHz

 

 

 

----------------------------------------------------------------------------------------

  Function           Time used/vector   input type                   vector length

- arm_mult_f32         -  0.775 us ; // real float32                    8

- arm_mult_f32         -  4.340 us ; // real float32                   64

- arm_mult_f32         - 15.000 us ; // real float32                  256

- arm_mult_f32         - 59.400 us ; // real float32                 1024

 

- arm_mult_q31         -  0.950 us ; // real q31                        8

- arm_mult_q31         -  5.280 us ; // real q31                       64

- arm_mult_q31         - 16.467 us ; // real q31                      256

- arm_mult_q31         - 64.800 us ; // real q31                     1024

 

- arm_mult_q15         -  0.680 us ; // real q15                        8

- arm_mult_q15         -  3.500 us ; // real q15                       64

- arm_mult_q15         - 11.000 us ; // real q15                      256

- arm_mult_q15         - 43.200 us ; // real q15                     1024

 

----------------------------------------------------------------------------------------

  Function           Time used/sample   input type

- sin                  -  0.880 us ; // real float32

- arm_sin_f32          -  0.480 us ; // real float32

- arm_sin_q31          -  0.393 us ; // real q31_t

- arm_sin_q15          -  0.286 us ; // real q15_t

- arm_sin_cos_f32      -  1.250 us ; // real float32

- arm_sin_cos_q31      -  1.910 us ; // real q31_t

- cos                  -  0.885 us ; // real float32

- arm_cos_f32          -  0.513 us ; // real float32

- arm_cos_q31          -  0.420 us ; // real q31_t

- arm_cos_q15          -  0.328 us ; // real q15_t

 

----------------------------------------------------------------------------------------

  Filter type          Time used/sample    input type           Taps Samples

- arm_fir_f32          -  3.080 us ; //   real float32           20      1

- arm_fir_f32          -  0.910 us ; //   real float32           20     20

- arm_fir_f32          -  0.673 us ; //   real float32           20     40

- arm_fir_f32          -  0.650 us ; //   real float32           20     80

 

- arm_fir_f32          -  5.280 us ; //   real float32           40      1

- arm_fir_f32          -  1.620 us ; //   real float32           40     20

- arm_fir_f32          -  1.155 us ; //   real float32           40     40

- arm_fir_f32          -  1.125 us ; //   real float32           40     80

 

- arm_fir_f32          -  9.840 us ; //   real float32           80      1

- arm_fir_f32          -  3.210 us ; //   real float32           80     20

- arm_fir_f32          -  2.183 us ; //   real float32           80     40

- arm_fir_f32          -  2.144 us ; //   real float32           80     80

 

- arm_fir_q31          -  4.680 us ; //   real q31_t             20      1

- arm_fir_q31          -  3.190 us ; //   real q31_t             20     20

- arm_fir_q31          -  3.150 us ; //   real q31_t             20     40

- arm_fir_q31          -  3.112 us ; //   real q31_t             20     80

 

- arm_fir_q31          -  8.333 us ; //   real q31_t             40      1

- arm_fir_q31          -  6.033 us ; //   real q31_t             40     20

- arm_fir_q31          -  5.933 us ; //   real q31_t             40     40

- arm_fir_q31          -  5.911 us ; //   real q31_t             40     80

 

- arm_fir_q31          - 15.800 us ; //   real q31_t             80      1

- arm_fir_q31          - 11.700 us ; //   real q31_t             80     20

- arm_fir_q31          - 11.550 us ; //   real q31_t             80     40

- arm_fir_q31          - 11.500 us ; //   real q31_t             80     80

 

- arm_fir_fast_q31     -  6.240 us ; //   real q31_t             20      1

- arm_fir_fast_q31     -  0.885 us ; //   real q31_t             20     20

- arm_fir_fast_q31     -  0.785 us ; //   real q31_t             20     40

- arm_fir_fast_q31     -  0.729 us ; //   real q31_t             20     80

 

- arm_fir_fast_q31     - 11.440 us ; //   real q31_t             40      1

- arm_fir_fast_q31     -  1.520 us ; //   real q31_t             40     20

- arm_fir_fast_q31     -  1.330 us ; //   real q31_t             40     40

- arm_fir_fast_q31     -  1.237 us ; //   real q31_t             40     80

 

- arm_fir_fast_q31     - 21.800 us ; //   real q31_t             80      1

- arm_fir_fast_q31     -  2.770 us ; //   real q31_t             80     20

- arm_fir_fast_q31     -  2.417 us ; //   real q31_t             80     40

- arm_fir_fast_q31     -  2.244 us ; //   real q31_t             80     80

 

- arm_fir_q15          -  2.640 us ; //   real q15_t             20      1

- arm_fir_q15          -  0.945 us ; //   real q15_t             20     20

- arm_fir_q15          -  0.905 us ; //   real q15_t             20     40

- arm_fir_q15          -  0.885 us ; //   real q15_t             20     80

 

- arm_fir_q15          -  4.178 us ; //   real q15_t             40      1

- arm_fir_q15          -  1.650 us ; //   real q15_t             40     20

- arm_fir_q15          -  1.585 us ; //   real q15_t             40     40

- arm_fir_q15          -  1.560 us ; //   real q15_t             40     80

 

- arm_fir_q15          -  7.333 us ; //   real q15_t             80      1

- arm_fir_q15          -  3.058 us ; //   real q15_t             80     20

- arm_fir_q15          -  2.958 us ; //   real q15_t             80     40

- arm_fir_q15          -  2.817 us ; //   real q15_t             80     80

 

- arm_fir_fast_q15     -  2.700 us ; //   real q15_t             20      1

- arm_fir_fast_q15     -  0.423 us ; //   real q15_t             20     20

- arm_fir_fast_q15     -  0.385 us ; //   real q15_t             20     40

- arm_fir_fast_q15     -  0.367 us ; //   real q15_t             20     80

 

- arm_fir_fast_q15     -  4.560 us ; //   real q15_t             40      1

- arm_fir_fast_q15     -  0.690 us ; //   real q15_t             40     20

- arm_fir_fast_q15     -  0.635 us ; //   real q15_t             40     40

- arm_fir_fast_q15     -  0.606 us ; //   real q15_t             40     80

 

- arm_fir_fast_q15     -  8.333 us ; //   real q15_t             80      1

- arm_fir_fast_q15     -  1.230 us ; //   real q15_t             80     20

- arm_fir_fast_q15     -  1.133 us ; //   real q15_t             80     40

- arm_fir_fast_q15     -  1.075 us ; //   real q15_t             80     80

 

----------------------------------------------------------------------------------------

  Filter type                       Time used/sample    input type           sections Samples

- arm_biquad_cascade_df1_f32        -  0.924 us ; //   real float32_t          1      1

- arm_biquad_cascade_df1_f32        -  0.195 us ; //   real float32_t          1     20

- arm_biquad_cascade_df1_f32        -  0.178 us ; //   real float32_t          1     40

- arm_biquad_cascade_df1_f32        -  0.170 us ; //   real float32_t          1     80

 

- arm_biquad_cascade_df1_f32        -  1.536 us ; //   real float32_t          2      1

- arm_biquad_cascade_df1_f32        -  0.377 us ; //   real float32_t          2     20

- arm_biquad_cascade_df1_f32        -  0.350 us ; //   real float32_t          2     40

- arm_biquad_cascade_df1_f32        -  0.336 us ; //   real float32_t          2     80

 

- arm_biquad_cascade_df1_f32        -  2.067 us ; //   real float32_t          3      1

- arm_biquad_cascade_df1_f32        -  0.553 us ; //   real float32_t          3     20

- arm_biquad_cascade_df1_f32        -  0.520 us ; //   real float32_t          3     40

- arm_biquad_cascade_df1_f32        -  0.502 us ; //   real float32_t          3     80

 

- arm_biquad_cascade_df1_fast_q31   -  1.690 us ; //   real q31_t              1      1

- arm_biquad_cascade_df1_fast_q31   -  0.382 us ; //   real q31_t              1     20

- arm_biquad_cascade_df1_fast_q31   -  0.347 us ; //   real q31_t              1     40

- arm_biquad_cascade_df1_fast_q31   -  0.330 us ; //   real q31_t              1     80

 

- arm_biquad_cascade_df1_fast_q31   -  2.850 us ; //   real q31_t              2      1

- arm_biquad_cascade_df1_fast_q31   -  0.740 us ; //   real q31_t              2     20

- arm_biquad_cascade_df1_fast_q31   -  0.683 us ; //   real q31_t              2     40

- arm_biquad_cascade_df1_fast_q31   -  0.655 us ; //   real q31_t              2     80

 

- arm_biquad_cascade_df1_fast_q31   -  4.000 us ; //   real q31_t              3      1

- arm_biquad_cascade_df1_fast_q31   -  1.095 us ; //   real q31_t              3     20

- arm_biquad_cascade_df1_fast_q31   -  1.015 us ; //   real q31_t              3     40

- arm_biquad_cascade_df1_fast_q31   -  0.975 us ; //   real q31_t              3     80

 

- arm_biquad_cascade_df1_q31        -  1.076 us ; //   real q31_t              1      1

- arm_biquad_cascade_df1_q31        -  0.205 us ; //   real q31_t              1     20

- arm_biquad_cascade_df1_q31        -  0.180 us ; //   real q31_t              1     40

- arm_biquad_cascade_df1_q31        -  0.169 us ; //   real q31_t              1     80

 

- arm_biquad_cascade_df1_q31        -  1.647 us ; //   real q31_t              2      1

- arm_biquad_cascade_df1_q31        -  0.383 us ; //   real q31_t              2     20

- arm_biquad_cascade_df1_q31        -  0.347 us ; //   real q31_t              2     40

- arm_biquad_cascade_df1_q31        -  0.332 us ; //   real q31_t              2     80

 

- arm_biquad_cascade_df1_q31        -  2.220 us ; //   real q31_t              3      1

- arm_biquad_cascade_df1_q31        -  0.563 us ; //   real q31_t              3     20

- arm_biquad_cascade_df1_q31        -  0.512 us ; //   real q31_t              3     40

- arm_biquad_cascade_df1_q31        -  0.493 us ; //   real q31_t              3     80

 

----------------------------------------------------------------------------------------

  Type                   Time used         input type                   length

- arm_cfft_radix2_q15  -   40.8 us ; // real q15_t                         64

- arm_cfft_radix2_q15  -  199.0 us ; // real q15_t                        256

- arm_cfft_radix2_q15  -  940.0 us ; // real q15_t                       1024

 

- arm_cfft_radix2_q31  -  119.6 us ; // real q31_t                         64

- arm_cfft_radix2_q31  -  608.3 us ; // real q31_t                        256

- arm_cfft_radix2_q31  - 2970.0 us ; // real q31_t                       1024

 

- arm_cfft_radix2_f32  -   62.5 us ; // real float32_t                     64

- arm_cfft_radix2_f32  -  327.0 us ; // real float32_t                    256

- arm_cfft_radix2_f32  - 1615.0 us ; // real float32_t                   1024

 

- arm_cfft_radix4_q15  -   28.5 us ; // real q15_t                         64

- arm_cfft_radix4_q15  -  150.5 us ; // real q15_t                        256

- arm_cfft_radix4_q15  -  755.0 us ; // real q15_t                       1024

 

- arm_cfft_radix4_q31  -   74.6 us ; // real q31_t                         64

- arm_cfft_radix4_q31  -  411.7 us ; // real q31_t                        256

- arm_cfft_radix4_q31  - 2100.0 us ; // real q31_t                       1024

 

- arm_cfft_radix4_f32  -   41.0 us ; // real float32_t                     64

- arm_cfft_radix4_f32  -  221.0 us ; // real float32_t                    256

- arm_cfft_radix4_f32  - 1110.0 us ; // real float32_t                   1024

 

----------------------------------------------------------------------------------------

Original Attachment has been moved to: DSP_pre_test.zip

Labels (1)
Tags (3)
2 Replies

3,366 Views
ramaprabhachock
Contributor I

Hi Poul,

I am working on ARM Cortex-M4 and was looking for a FPU benchmark test. I found your test and downloaded it. Thanks for putting it on this link.

When I tried to compile, I found that the functions _time_get(), _time_diff(), the structure type TIME_STRUCT are not available in the library files which you have included (math.h/arm_math.h). Where are they located? Are they customized functions written by you?

Also, have you compared the figures which you have shown here with any reference values?

Please clarify.

Thanks,

Best regards,
Rama 

0 Kudos
Reply

3,366 Views
takmingmarcopan
Contributor II

This is a bit late but the TIME_STRUCT is actually part of the MQX RTOS. 
It is used as an object tied to the system 32-bit clock iirc. 

0 Kudos
Reply