K70 Can module: 32 or 64 mailbox?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K70 Can module: 32 or 64 mailbox?

ソリューションへジャンプ
1,926件の閲覧回数
arnogir
Senior Contributor II

Hello

I'm using the K70 150MHz with MQX 4.2 and KDS.

The datasheet of the K70 (Rev.3 November 2014) indicate only the register CANx_IMASK1/ CANx_IFLAG1, not the IMASK2/IFLAG2...

But in KDS3.0 with EmbSys Register I can visualise  IFLAG2/IMASK2.

But on Can Clock Turn on in BSP init (sim->SCGC6 |= SIM_SCGC6_FLEXCAN0_MASK;)

only IFLAG1/IMASK1 are set to 0, IMASK2/IFLAG 2 not change and MASK2 stay to 0x80008000???

Also, in Datasheet §53.3.12 (CANx_CTRL2) on RFFN description, there is a table indicate how many remaining available mailboxes which can up to 64...

:smileyconfused:

So if there is realy 64 Maibox, the Clock turn on allow automaticcaly to Reset MASK/IFLAG1 to 0 but not the IMASK2/IFLAG2, in which case, MQX 4.2 has a bug by not setting the default value register to 0..?

So are they 32 or 64 mb in K70

0 件の賞賛
返信
1 解決策
1,773件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

K70 has two identical FlexCAN  modules.

Each FlexCAN module contains 16 message buffers.Wish it helps

Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,774件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

K70 has two identical FlexCAN  modules.

Each FlexCAN module contains 16 message buffers.Wish it helps

Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,773件の閲覧回数
arnogir
Senior Contributor II

Ok,

I just saw this in the chapter §3.9.4 CAN Configuration

Thank you:smileyhappy:

0 件の賞賛
返信