K66 port size 32 bits and 16bits hardware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K66 port size 32 bits and 16bits hardware

887 次查看
thaophan
Contributor II

Hi every one

In my hardware I connect K66 to SDRAM via 32 bit port and 8 column adrress lines interface , but It doesn't work. Now, I want to replace 32bits SDRAM with 16 bits SDRAM. Can it works with my hardware connection.

Thank in advance.

1 回复

789 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The K66 SDRAM controller supports 32-bit port and 8-Column address lines with below connection:

pastedImage_1.png

Please check if your connection match with above requirement.

And K66 SDRAM controller also supports 16-bit port and 8-Column SDRAM device with below connection:

pastedImage_2.png

Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------