K66 high speed mode and Flash programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K66 high speed mode and Flash programming

1,558件の閲覧回数
PeterFromSweden
Contributor III

Hi

When I try to perform flash erase on K66 in high speed mode, 180 MHz, I get ACCERR set. This seems to be caused by high speed mode and works fine when I run at 120 MHz.

This is hard to find in reference manual (if it is at all like that).

Regards

/Peter

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,381件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Peter Liedholm:

Your assumption is correct, and it is mentioned in the Reference Manual:

pastedImage_0.png

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信