K66 high speed mode and Flash programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K66 high speed mode and Flash programming

1,540 Views
PeterFromSweden
Contributor III

Hi

When I try to perform flash erase on K66 in high speed mode, 180 MHz, I get ACCERR set. This seems to be caused by high speed mode and works fine when I run at 120 MHz.

This is hard to find in reference manual (if it is at all like that).

Regards

/Peter

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,363 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Peter Liedholm:

Your assumption is correct, and it is mentioned in the Reference Manual:

pastedImage_0.png

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply