K66 high speed mode and Flash programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K66 high speed mode and Flash programming

1,585 次查看
PeterFromSweden
Contributor III

Hi

When I try to perform flash erase on K66 in high speed mode, 180 MHz, I get ACCERR set. This seems to be caused by high speed mode and works fine when I run at 120 MHz.

This is hard to find in reference manual (if it is at all like that).

Regards

/Peter

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,408 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Peter Liedholm:

Your assumption is correct, and it is mentioned in the Reference Manual:

pastedImage_0.png

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复