K66 SDRAM always addressing same location

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K66 SDRAM always addressing same location

1,071件の閲覧回数
jch4416
Contributor I

Hello,

I'm using a MK66FX1M0VMD18 with a 16bit  AS4C4M16SA-TIN SDRAM. The SDRAM has 8 column addresses, so the connections between it and the K66 are the same as in Table 35-7 of the K66 Family Reference Manual, with A21-22 on the K66 going to BA0-1 on the SDRAM.

The problem we are having is that if I write a value to a specific address, then I will get that same value back for every address that I then read.  So it is essentially as if the SDRAM controller ignores the address in the CPU instruction and always accesses the same SDRAM location. 

Has anyone seen this isssue before?

Thanks,

Jim

0 件の賞賛
返信
1 返信

986件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Jim,

The K66 chip provides the cache for SDRAM memory with below setting:

pastedImage_1.png

Please check if the cache was enabled at your application.

If yes, you could try to close the cache and check the issue again.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信