K66 SDRAM Interface connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K66 SDRAM Interface connection

1,433 次查看
eico
Contributor I

How should I go about hooking up the SDRAM addressing lines from the K66 to the Micron part MT48LC4M16A2B4-6A IT? I am having trouble figuring it out from the K66 RM. It is a 64Mb SDRAM module organized as 1Mb x 16 x 4 banks. There are 8 column addresses, with 12 address pins and 2 bank select pins. This doesn’t match any of the specific examples in the RM, and I’m not sure I understand it well enough to hook it up right. My best guess would be as follows:

 

SDRAM Controller Pins:

A9

A10

A11

A12

A13

A14

A15

A16

A17

A18

A19

A20

A21

A22

SDRAM Pins:

A7

A6

A5

A4

A3

A2

A1

A0

A8

A9

A10

A11

BA0

BA1

 

Is that accurate?”

0 项奖励
回复
1 回复

1,262 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Customer need to refer Table 35-7 about MT48LC4M16A2B4-6A SDRAM connection:

pastedImage_1.png

Customer connection is correct:

pastedImage_2.png


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复