K66 - Problems programming flash.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K66 - Problems programming flash.

Jump to solution
3,692 Views
calvinday
Contributor III

We have written a bootloader that occupies the 0x000000 - 0x0FFFFF in flash memory and a application that occupies 0x100000 - 0x1FFFFF.

When the bootloader runs, it checks to see if the application is in flash. If not, it will copy the application from external eMMC and flash it. The unit then reboots and the bootloader launches the new application.

Everything is working as expected however, when we moved the application to location 0x06000 - 0x1FFFFF, the flash erase function no longer works while trying to erase the first sector. While debugging, the MCU appears to restart.

We are using KDS 2.0.

What could be wrong?

0 Kudos
Reply
1 Solution
3,539 Views
ndavies
Contributor V

Did you disable all interrupts or move the active interrupts executable and remap the vectors to RAM? Interrupts must not jump to a flash bank code when you're trying to flash it.

View solution in original post

0 Kudos
Reply
4 Replies
3,539 Views
calvinday
Contributor III

I thought we had to provide copy functions to ram functions but it is done automatically using

FLASH_DRIVER_IS_FLASH_RESIDENT.

0 Kudos
Reply
3,539 Views
calvinday
Contributor III

We realized that the code must be run out of ram so we added some relocated flash functions to ram.

0 Kudos
Reply
3,540 Views
ndavies
Contributor V

Did you disable all interrupts or move the active interrupts executable and remap the vectors to RAM? Interrupts must not jump to a flash bank code when you're trying to flash it.

0 Kudos
Reply
3,539 Views
calvinday
Contributor III

The MCU is resetting and the RCM_SRS1 register reports a LOCKUP event.

0 Kudos
Reply