K66 Pinout ADC0_DP0 not found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K66 Pinout ADC0_DP0 not found

跳至解决方案
1,577 次查看
jayas
Contributor I

I want to use differential ADC in K66 uC, but I only found one of the two ADCs ports because the negative pair to use with pin 28 is not in the datasheet.

I have ADC0_DM0 or ADC1_DM3 on pin 28 (L2) but I cann`t find ADC0_DP0 or ADC1_DP3 

0 项奖励
回复
1 解答
1,457 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Juan,

For the K66, the ADC0_DP0 is not available for differential inputs. Only the pins 29 and 30 can be used as differential inputs and are shared between ADC0 and ADC1.

The inputs are ADC0_DP3 and ADC0_DM3 for ADC0 channel 3 and ADC1_DP0 and ADC1_DM0 for ADC1.

pastedImage_1.png

Best Regards,

Gerardo

在原帖中查看解决方案

3 回复数
1,458 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Juan,

For the K66, the ADC0_DP0 is not available for differential inputs. Only the pins 29 and 30 can be used as differential inputs and are shared between ADC0 and ADC1.

The inputs are ADC0_DP3 and ADC0_DM3 for ADC0 channel 3 and ADC1_DP0 and ADC1_DM0 for ADC1.

pastedImage_1.png

Best Regards,

Gerardo

1,457 次查看
jayas
Contributor I

Thank you Gerardo. It means than we can only use 1 differential ADC input un this model, isn't?

Only if we found an exernal multiplexing device to switch between channels we can use ADC0 and AD1 sharing same pins.

0 项奖励
回复
1,457 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Juan,

It is correct. Only one differential ADC input is available for the K66, but you could use an external analog multiplexer to extend this capability.

0 项奖励
回复