K66 CAN INT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K66 CAN INT

跳至解决方案
3,625 次查看
j_cfernandez
Contributor II

We took over the project from K60 to K66. With the same initialization, the interrrupt no longer works. What is the difference.

标签 (1)
0 项奖励
回复
1 解答
3,261 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I checked the CAN0 and CAN1 interrupt setting code with problem.

As ARM Cortex M4 core shows the interrupt set-enable registers shows the IRQ number (IRQ) with related register:

2015-12-22_13-14-42.png

For the CAN0 interrupt IRQ value from 75 to 80, which need to use NVIC_ISER2 register to enable CAN0 interrupt.

The CAN1 interrupt IRQ value from 94 to 99, which need to use NVIC_ISER2 and NVIC_ISER3 to enable related CAN1 interrupt.

Please refer below code, which is for K70_120MHz product to enable interrupt function:

/***********************************************************************/

/*

* Initialize the NVIC to enable the specified IRQ.

*

* NOTE: The function only initializes the NVIC to enable a single IRQ.

* Interrupts will also need to be enabled in the ARM core. This can be

* done using the EnableInterrupts macro.

*

* Parameters:

* irq    irq number to be enabled (the irq number NOT the vector number)

*/

void enable_irq (int irq)

{

    int div;

   

    /* Make sure that the IRQ is an allowable number. Right now up to 105 is

     * used.

     */

    if (irq > 105)

        printf("\nERR! Invalid IRQ value passed to enable irq function!\n");

   

    /* Determine which of the NVICISERs corresponds to the irq */

    div = irq/32;

   

    switch (div)

    {

        case 0x0:

              NVICICPR0 |= 1 << (irq%32);

              NVICISER0 |= 1 << (irq%32);

              break;

        case 0x1:

              NVICICPR1 |= 1 << (irq%32);

              NVICISER1 |= 1 << (irq%32);

              break;

        case 0x2:

              NVICICPR2 |= 1 << (irq%32);

              NVICISER2 |= 1 << (irq%32);

              break;

    case 0x3:

          NVICICPR3 |= 1 << (irq%32);

          NVICISER3 |= 1 << (irq%32);

          break;

    }             

}

Wish it helps.

Best regards,

Ma Hui

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,261 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

If you are using K60_120MHz product and port to K66 product, the interrupt vector assignment has changed:

K60_120MHz product CAN0 interrupt vector from 45 to 50, CAN1 interrupt vector from 53 to 58;

K66 product CAN0 interrupt vector from 91 to 96, CAN1 interrupt vector from 110 to 115;

More detailed info, please check each reference manual chapter3.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,261 次查看
j_cfernandez
Contributor II

Hi,

thanks for the answers.

I set the numbers correctly. But doesn't work. In the Register i can see the data.

Here my init Code:

MK66F18.h

[...]

  CAN0_ORed_Message_buffer_IRQn = 75,              /**< CAN0 OR'd message buffers interrupt */

  CAN0_Bus_Off_IRQn            = 76,               /**< CAN0 bus off interrupt */

  CAN0_Error_IRQn              = 77,               /**< CAN0 error interrupt */

  CAN0_Tx_Warning_IRQn         = 78,               /**< CAN0 Tx warning interrupt */

  CAN0_Rx_Warning_IRQn         = 79,               /**< CAN0 Rx warning interrupt */

  CAN0_Wake_Up_IRQn            = 80,               /**< CAN0 wake up interrupt */

[..]

  CAN1_ORed_Message_buffer_IRQn = 94,              /**< CAN1 OR'd message buffers interrupt */

  CAN1_Bus_Off_IRQn            = 95,               /**< CAN1 bus off interrupt */

  CAN1_Error_IRQn              = 96,               /**< CAN1 error interrupt */

  CAN1_Tx_Warning_IRQn         = 97,               /**< CAN1 Tx warning interrupt */

  CAN1_Rx_Warning_IRQn         = 98,               /**< CAN1 Rx warning interrupt */

  CAN1_Wake_Up_IRQn            = 99                /**< CAN1 wake up interrupt */

[...]

I init the Can 1 and 2:

  CANX->CTRL1 &= ~(CAN_CTRL1_CLKSRC_MASK); CTRL1[CLK_SRC] bit. (OSCCLK) 
  CANX->MCR   &= ~(CAN_MCR_MDIS_MASK);
  while((CAN_MCR_LPMACK_MASK & CANX->MCR));
  while(!(CAN_MCR_FRZACK_MASK & CANX->MCR));

  CANX->MCR |=    CAN_MCR_IRMQ_MASK;
  CANX->MCR |=    CAN_MCR_WRNEN_MASK;
  CANX->MCR &=  ~(CAN_MCR_SRXDIS_MASK);
  CANX->MCR |=    CAN_MCR_AEN_MASK;
  CANX->MCR |=    CAN_MCR_LPRIOEN_MASK;
  can_init_BAUD( baudrateKHz , X , 12000000 ); 

I init the CAN 0 Int.:

  NVIC->ICPR[ 0 ] = ( NVIC->ICPR[ 0 ] & ~(((uint32_t)0x07)<<29)) | (((uint32_t)0x07)<<29);  /* Clear pending interrupt CAN0 */

  NVIC->ISER[ 0 ] = ( NVIC->ISER[ 0 ] & ~(((uint32_t)0x07)<<29)) | (((uint32_t)0x07)<<29);  /* enable interrupt CAN0 */

  NVIC->ICPR[ 1 ] = ( NVIC->ICPR[ 1 ] & ~(((uint32_t)0x1F)<<0))  | ((uint32_t)0x1F);   /* Clear pending interrupt CAN0 */

  NVIC->ISER[ 1 ] = ( NVIC->ISER[ 1 ] & ~(((uint32_t)0x1F)<<0))  | ((uint32_t)0x1F);    /* enable interrupt CAN0 */

I init the CAN 1 Int.:

  NVIC->ICPR[ 1 ] = ( NVIC->ICPR[ 1 ] & ~(((uint32_t)0xFF)<<5))  | (((uint32_t)0xFF)<<5);  /* Clear pending interrupt CAN1*/

  NVIC->ISER[ 1 ] = ( NVIC->ISER[ 1 ] & ~(((uint32_t)0xFF)<<5))  | (((uint32_t)0xFF)<<5);  /* enable interrupt CAN1*/

0 项奖励
回复
3,262 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I checked the CAN0 and CAN1 interrupt setting code with problem.

As ARM Cortex M4 core shows the interrupt set-enable registers shows the IRQ number (IRQ) with related register:

2015-12-22_13-14-42.png

For the CAN0 interrupt IRQ value from 75 to 80, which need to use NVIC_ISER2 register to enable CAN0 interrupt.

The CAN1 interrupt IRQ value from 94 to 99, which need to use NVIC_ISER2 and NVIC_ISER3 to enable related CAN1 interrupt.

Please refer below code, which is for K70_120MHz product to enable interrupt function:

/***********************************************************************/

/*

* Initialize the NVIC to enable the specified IRQ.

*

* NOTE: The function only initializes the NVIC to enable a single IRQ.

* Interrupts will also need to be enabled in the ARM core. This can be

* done using the EnableInterrupts macro.

*

* Parameters:

* irq    irq number to be enabled (the irq number NOT the vector number)

*/

void enable_irq (int irq)

{

    int div;

   

    /* Make sure that the IRQ is an allowable number. Right now up to 105 is

     * used.

     */

    if (irq > 105)

        printf("\nERR! Invalid IRQ value passed to enable irq function!\n");

   

    /* Determine which of the NVICISERs corresponds to the irq */

    div = irq/32;

   

    switch (div)

    {

        case 0x0:

              NVICICPR0 |= 1 << (irq%32);

              NVICISER0 |= 1 << (irq%32);

              break;

        case 0x1:

              NVICICPR1 |= 1 << (irq%32);

              NVICISER1 |= 1 << (irq%32);

              break;

        case 0x2:

              NVICICPR2 |= 1 << (irq%32);

              NVICISER2 |= 1 << (irq%32);

              break;

    case 0x3:

          NVICICPR3 |= 1 << (irq%32);

          NVICISER3 |= 1 << (irq%32);

          break;

    }             

}

Wish it helps.

Best regards,

Ma Hui

0 项奖励
回复
3,261 次查看
j_cfernandez
Contributor II

Dear,

it`s working fine.

Thank you

0 项奖励
回复
3,261 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Please tell us the whole part number of the two chips.

And please describe detail about your project , and how to porting it 。 You'd better provide the project .

BR

Alice

0 项奖励
回复