K65F and KV58F Crystal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K65F and KV58F Crystal

1,755件の閲覧回数
a8Chcx
Contributor V

Hi,

I am using 50MHz on XTAL0 input and leave EXTAL0 unconnected on K64F, and works fine.

1. Can I do the same on K65F or I have to use 8MHz, 12MHZ or 16MHz on XTAL0 & EXTAL0? Why?

2. How about KV58F? Looks like I can use 50MHz because 50MHz is used on TWR-KV58F?

Thanks,

Christie

0 件の賞賛
返信
3 返答(返信)

1,597件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Christie,

1. Can I do the same on K65F or I have to use 8MHz, 12MHZ or 16MHz on XTAL0 & EXTAL0? Why?

The K65F also support the 50 MHz external clock.

2016-05-05_9-41-06.jpg

2. How about KV58F? Looks like I can use 50MHz because 50MHz is used on TWR-KV58F?

Yes, the 50 MHz external oscillator can directly drive the EXTAL pin.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,597件の閲覧回数
a8Chcx
Contributor V

Hi Ping,

I checked the data sheet of K65F(Page 118). It says:

NOTE

In order to lock HS USB PHY PLL clock and make the

integrated HS USB PHY working, external clock on EXTAL0

or external crystal connected to system oscillator should be one

of the following values: 12MHz, 16MHz or 24MHz.

So, looks like that I can't use 50MHz if I want to use HS USB? Otherwise, it is fine with 50MHz external crystal?

Thanks,

Christie

0 件の賞賛
返信

1,597件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Christie,

From the perspective, your understand is correct.

Hope it helps.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信